SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
Table 11-33 lists the memory-mapped registers for the FCFG1 registers. All register offset addresses not listed in Table 11-33 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Section |
---|---|---|---|
A0h | MISC_CONF_1 | Misc configurations | Section 11.4.1 |
A4h | MISC_CONF_2 | Internal | Section 11.4.2 |
B0h | HPOSC_MEAS_5 | Internal | Section 11.4.3 |
B4h | HPOSC_MEAS_4 | Internal | Section 11.4.4 |
B8h | HPOSC_MEAS_3 | Internal | Section 11.4.5 |
BCh | HPOSC_MEAS_2 | Internal | Section 11.4.6 |
C0h | HPOSC_MEAS_1 | Internal | Section 11.4.7 |
C4h | CONFIG_CC26_FE | Internal | Section 11.4.8 |
C8h | CONFIG_CC13_FE | Internal | Section 11.4.9 |
CCh | CONFIG_RF_COMMON | Internal | Section 11.4.10 |
D0h | CONFIG_SYNTH_DIV2_CC26_2G4 | Internal | Section 11.4.11 |
D4h | CONFIG_SYNTH_DIV2_CC13_2G4 | Internal | Section 11.4.12 |
D8h | CONFIG_SYNTH_DIV2_CC26_1G | Internal | Section 11.4.13 |
DCh | CONFIG_SYNTH_DIV2_CC13_1G | Internal | Section 11.4.14 |
E0h | CONFIG_SYNTH_DIV4_CC26 | Internal | Section 11.4.15 |
E4h | CONFIG_SYNTH_DIV4_CC13 | Internal | Section 11.4.16 |
E8h | CONFIG_SYNTH_DIV5 | Internal | Section 11.4.17 |
ECh | CONFIG_SYNTH_DIV6_CC26 | Internal | Section 11.4.18 |
F0h | CONFIG_SYNTH_DIV6_CC13 | Internal | Section 11.4.19 |
F4h | CONFIG_SYNTH_DIV10 | Internal | Section 11.4.20 |
F8h | CONFIG_SYNTH_DIV12_CC26 | Internal | Section 11.4.21 |
FCh | CONFIG_SYNTH_DIV12_CC13 | Internal | Section 11.4.22 |
100h | CONFIG_SYNTH_DIV15 | Internal | Section 11.4.23 |
104h | CONFIG_SYNTH_DIV30 | Internal | Section 11.4.24 |
144h | IOCONF | IO Configuration | Section 11.4.25 |
294h | USER_ID | User Identification. | Section 11.4.26 |
2B0h | FLASH_OTP_DATA3 | Internal | Section 11.4.27 |
2B4h | ANA2_TRIM | Internal | Section 11.4.28 |
2B8h | LDO_TRIM | Internal | Section 11.4.29 |
2E8h | MAC_BLE_0 | MAC BLE Address 0 | Section 11.4.30 |
2ECh | MAC_BLE_1 | MAC BLE Address 1 | Section 11.4.31 |
2F0h | MAC_15_4_0 | MAC IEEE 802.15.4 Address 0 | Section 11.4.32 |
2F4h | MAC_15_4_1 | MAC IEEE 802.15.4 Address 1 | Section 11.4.33 |
30Ch | MISC_TRIM | Miscellaneous Trim Parameters | Section 11.4.34 |
310h | RCOSC_HF_TEMPCOMP | Internal | Section 11.4.35 |
318h | ICEPICK_DEVICE_ID | IcePick Device Identification | Section 11.4.36 |
31Ch | FCFG1_REVISION | Factory Configuration (FCFG1) Revision | Section 11.4.37 |
320h | MISC_OTP_DATA | Misc OTP Data | Section 11.4.38 |
34Ch | CONFIG_IF_ADC | Internal | Section 11.4.39 |
350h | CONFIG_OSC_TOP | Internal | Section 11.4.40 |
35Ch | SOC_ADC_ABS_GAIN | AUX_ADC Gain in Absolute Reference Mode | Section 11.4.41 |
360h | SOC_ADC_REL_GAIN | AUX_ADC Gain in Relative Reference Mode | Section 11.4.42 |
368h | SOC_ADC_OFFSET_INT | AUX_ADC Temperature Offsets in Absolute Reference Mode | Section 11.4.43 |
36Ch | SOC_ADC_REF_TRIM_AND_OFFSET_EXT | Internal | Section 11.4.44 |
370h | AMPCOMP_TH1 | Internal | Section 11.4.45 |
374h | AMPCOMP_TH2 | Internal | Section 11.4.46 |
378h | AMPCOMP_CTRL1 | Internal | Section 11.4.47 |
37Ch | ANABYPASS_VALUE2 | Internal | Section 11.4.48 |
388h | VOLT_TRIM | Internal | Section 11.4.49 |
38Ch | OSC_CONF | OSC Configuration | Section 11.4.50 |
390h | FREQ_OFFSET | Internal | Section 11.4.51 |
398h | MISC_OTP_DATA_1 | Internal | Section 11.4.52 |
3D0h | SHDW_DIE_ID_0 | Shadow of EFUSE:DIE_ID_0 register | Section 11.4.53 |
3D4h | SHDW_DIE_ID_1 | Shadow of EFUSE:DIE_ID_1 register | Section 11.4.54 |
3D8h | SHDW_DIE_ID_2 | Shadow of EFUSE:DIE_ID_2 register | Section 11.4.55 |
3DCh | SHDW_DIE_ID_3 | Shadow of EFUSE:DIE_ID_3 register | Section 11.4.56 |
3F8h | SHDW_SCAN_MCU3_SEC | Internal | Section 11.4.57 |
3FCh | SHDW_SCAN_DATA1_CRC | Internal | Section 11.4.58 |
404h | SHDW_ANA_TRIM | Internal | Section 11.4.59 |
408h | OSC_CONF1 | Oscillator configuration | Section 11.4.60 |
40Ch | DAC_BIAS_CNF | Internal | Section 11.4.61 |
418h | TFW_PROBE | Internal | Section 11.4.62 |
41Ch | TFW_FT | Internal | Section 11.4.63 |
420h | DAC_CAL0 | Internal | Section 11.4.64 |
424h | DAC_CAL1 | Internal | Section 11.4.65 |
428h | DAC_CAL2 | Internal | Section 11.4.66 |
42Ch | DAC_CAL3 | Internal | Section 11.4.67 |
Complex bit access types are encoded to fit into small table cells. Table 11-34 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
Reset or Default Value | ||
-n | Value after reset or the default value |
MISC_CONF_1 is shown in Table 11-35.
Return to the Summary Table.
Misc configurations
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | DEVICE_MINOR_REV | R | X | HW minor revision number (a value of 0xFF shall be treated equally to 0x00). Any test of this field by SW should be implemented as a 'greater or equal' comparison as signed integer. Value may change without warning. Default value holds log information from production test. |
MISC_CONF_2 is shown in Table 11-36.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | HPOSC_COMP_P3 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
HPOSC_MEAS_5 is shown in Table 11-37.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | HPOSC_D5 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
15-8 | HPOSC_T5 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
7-0 | HPOSC_DT5 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
HPOSC_MEAS_4 is shown in Table 11-38.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | HPOSC_D4 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
15-8 | HPOSC_T4 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
7-0 | HPOSC_DT4 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
HPOSC_MEAS_3 is shown in Table 11-39.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | HPOSC_D3 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
15-8 | HPOSC_T3 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
7-0 | HPOSC_DT3 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
HPOSC_MEAS_2 is shown in Table 11-40.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | HPOSC_D2 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
15-8 | HPOSC_T2 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
7-0 | HPOSC_DT2 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
HPOSC_MEAS_1 is shown in Table 11-41.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | HPOSC_D1 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
15-8 | HPOSC_T1 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
7-0 | HPOSC_DT1 | R | X | Internal. Only to be used through TI provided API. Default value holds log information from production test. |
CONFIG_CC26_FE is shown in Table 11-42.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | IFAMP_IB | R | 7h | Internal. Only to be used through TI provided API. |
27-24 | LNA_IB | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
23-19 | IFAMP_TRIM | R | 0h | Internal. Only to be used through TI provided API. |
18-14 | CTL_PA0_TRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
13 | PATRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
12 | RSSITRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-8 | RESERVED | R | 0h | Reserved |
7-0 | RSSI_OFFSET | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
CONFIG_CC13_FE is shown in Table 11-43.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | IFAMP_IB | R | 7h | Internal. Only to be used through TI provided API. |
27-24 | LNA_IB | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
23-19 | IFAMP_TRIM | R | 0h | Internal. Only to be used through TI provided API. |
18-14 | CTL_PA0_TRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
13 | PATRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
12 | RSSITRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-8 | RESERVED | R | 0h | Reserved |
7-0 | RSSI_OFFSET | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
CONFIG_RF_COMMON is shown in Table 11-44.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | DISABLE_CORNER_CAP | R | 1h | Internal. Only to be used through TI provided API. |
30-25 | SLDO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
24-22 | RESERVED | R | 0h | Reserved |
21 | PA20DBMTRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. |
20-16 | CTL_PA_20DBM_TRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
15-9 | RFLDO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. |
8-6 | QUANTCTLTHRES | R | 5h | Internal. Only to be used through TI provided API. |
5-0 | DACTRIM | R | Dh | Internal. Only to be used through TI provided API. |
CONFIG_SYNTH_DIV2_CC26_2G4 is shown in Table 11-45.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV2_CC13_2G4 is shown in Table 11-46.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV2_CC26_1G is shown in Table 11-47.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV2_CC13_1G is shown in Table 11-48.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV4_CC26 is shown in Table 11-49.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV4_CC13 is shown in Table 11-50.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV5 is shown in Table 11-51.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV6_CC26 is shown in Table 11-52.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV6_CC13 is shown in Table 11-53.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV10 is shown in Table 11-54.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV12_CC26 is shown in Table 11-55.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV12_CC13 is shown in Table 11-56.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV15 is shown in Table 11-57.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
CONFIG_SYNTH_DIV30 is shown in Table 11-58.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | MIN_ALLOWED_RTRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-12 | RFC_MDM_DEMIQMC0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-6 | LDOVCO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
5 | RFC_MDM_DEMIQMC0_TRIMCOMPLETE_N | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | RESERVED | R | 0h | Reserved |
IOCONF is shown in Table 11-59.
Return to the Summary Table.
IO Configuration
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-7 | RESERVED | R | 0h | Reserved |
6-0 | GPIO_CNT | R | X | Number of available DIOs. Default value differs depending on partnumber. |
USER_ID is shown in Table 11-60.
Return to the Summary Table.
User Identification.
Reading this register and the FCFG1:ICEPICK_DEVICE_ID register is the only supported way of identifying a device.
The value of this register will be written to AON_PMCTL:JTAGUSERCODE by boot FW while in safezone.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | PG_REV | R | 1h | Field used to distinguish revisions of the device |
27-26 | VER | R | X | Version number. 0x0: Bits [25:12] of this register has the stated meaning. Any other setting indicate a different encoding of these bits. Default value differs depending on partnumber. |
25 | PA | R | X | 0: Does not support 20dBm PA 1: Supports 20dBM PA Default value differs depending on partnumber. |
24 | RESERVED | R | 0h | Reserved |
23 | CC13 | R | X | 0: CC26x4x10 device type 1: CC13x4x10 device type Default value differs depending on partnumber. |
22-19 | SEQUENCE | R | X | Sequence. Used to differentiate between marketing/orderable product where other fields of this register are the same (temp range, flash size, voltage range etc) Default value differs depending on partnumber. |
18-16 | PKG | R | X | Package type. 0x2: 7x7mm QFN (RGZ) package 0x7: 8x8mm QFN (RSK) package Other values are reserved for future use. Packages available for a specific device are shown in the device datasheet. Default value differs depending on partnumber. |
15-12 | PROTOCOL | R | X | Protocols supported. 0x1: BLE 0x2: RF4CE 0x4: Zigbee/6lowpan 0x8: Proprietary More than one protocol can be supported on same device - values above are then combined. Default value differs depending on partnumber. |
11-0 | RESERVED | R | 0h | Reserved |
FLASH_OTP_DATA3 is shown in Table 11-61.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-3 | RESERVED | R | 0h | Reserved |
2-0 | FLASH_SIZE | R | X | Internal. Only to be used through TI provided API. Default value differs depending on partnumber. |
ANA2_TRIM is shown in Table 11-62.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | RCOSCHFCTRIMFRACT_EN | R | 1h | Internal. Only to be used through TI provided API. |
30-26 | RCOSCHFCTRIMFRACT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
25 | RESERVED | R | 0h | Reserved |
24-23 |
SET_RCOSC_HF_FINE_ RESISTOR | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
22 |
ATESTLF_UDIGLDO_ IBIAS_TRIM | R | 1h | Internal. Only to be used through TI provided API. |
21-15 | NANOAMP_RES_TRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
14-12 | DCDC_DRV_DS | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11 | DITHER_EN | R | 1h | Internal. Only to be used through TI provided API. |
10-8 | DCDC_IPEAK | R | 0h | Internal. Only to be used through TI provided API. |
7-6 | DEAD_TIME_TRIM | R | 1h | Internal. Only to be used through TI provided API. |
5-3 | DCDC_LOW_EN_SEL | R | 7h | Internal. Only to be used through TI provided API. |
2-0 | DCDC_HIGH_EN_SEL | R | 7h | Internal. Only to be used through TI provided API. |
LDO_TRIM is shown in Table 11-63.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-29 | RESERVED | R | 0h | Reserved |
28-24 | VDDR_TRIM_SLEEP | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
23-19 | RESERVED | R | 0h | Reserved |
18-16 | GLDO_CURSRC | R | 0h | Internal. Only to be used through TI provided API. |
15-13 | RESERVED | R | 0h | Reserved |
12-11 | ITRIM_DIGLDO_LOAD | R | 0h | Internal. Only to be used through TI provided API. |
10-8 | ITRIM_UDIGLDO | R | 0h | Internal. Only to be used through TI provided API. |
7-3 | RESERVED | R | 0h | Reserved |
2-0 | VTRIM_DELTA | R | 3h | Internal. Only to be used through TI provided API. |
MAC_BLE_0 is shown in Table 11-64.
Return to the Summary Table.
MAC BLE Address 0
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | ADDR_0_31 | R | X | The first 32-bits of the 64-bit MAC BLE address Default value holds trim value from production test. |
MAC_BLE_1 is shown in Table 11-65.
Return to the Summary Table.
MAC BLE Address 1
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | ADDR_32_63 | R | X | The last 32-bits of the 64-bit MAC BLE address Default value holds trim value from production test. |
MAC_15_4_0 is shown in Table 11-66.
Return to the Summary Table.
MAC IEEE 802.15.4 Address 0
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | ADDR_0_31 | R | X | The first 32-bits of the 64-bit MAC 15.4 address Default value holds trim value from production test. |
MAC_15_4_1 is shown in Table 11-67.
Return to the Summary Table.
MAC IEEE 802.15.4 Address 1
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | ADDR_32_63 | R | X | The last 32-bits of the 64-bit MAC 15.4 address Default value holds trim value from production test. |
MISC_TRIM is shown in Table 11-68.
Return to the Summary Table.
Miscellaneous Trim Parameters
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-17 | RESERVED | R | 0h | Reserved |
16-12 |
TRIM_RECHARGE_ COMP_OFFSET | R | X | Internal. Only to be used through TI provided API. |
11-8 |
TRIM_RECHARGE_ COMP_REFLEVEL | R | X | Internal. Only to be used through TI provided API. |
7-0 | TEMPVSLOPE | R | 3Bh | Signed byte value representing the TEMP slope with battery voltage, in degrees C / V, with four fractional bits. |
RCOSC_HF_TEMPCOMP is shown in Table 11-69.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-24 | FINE_RESISTOR | R | 0h | Internal. Only to be used through TI provided API. |
23-16 | CTRIM | R | 0h | Internal. Only to be used through TI provided API. |
15-8 | CTRIMFRACT_QUAD | R | 0h | Internal. Only to be used through TI provided API. |
7-0 | CTRIMFRACT_SLOPE | R | 3h | Internal. Only to be used through TI provided API. |
ICEPICK_DEVICE_ID is shown in Table 11-70.
Return to the Summary Table.
IcePick Device Identification
Reading this register and the FCFG1:USER_ID register is the only supported way of identifying a device.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | PG_REV | R | 1h | Field used to distinguish revisions of the device. |
27-12 | WAFER_ID | R | BB78h | Field used to identify silicon die. |
11-0 | MANUFACTURER_ID | R | 2Fh | Manufacturer code. 0x02F: Texas Instruments |
FCFG1_REVISION is shown in Table 11-71.
Return to the Summary Table.
Factory Configuration (FCFG1) Revision
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | REV | R | 2Ah | The revision number of the FCFG1 layout. This value will be read by application SW in order to determine which FCFG1 parameters that have valid values. This revision number must be incremented by 1 before any devices are to be produced if the FCFG1 layout has changed since the previous production of devices. Value migth change without warning. |
MISC_OTP_DATA is shown in Table 11-72.
Return to the Summary Table.
Misc OTP Data
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | RCOSC_HF_ITUNE | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
27-20 | RCOSC_HF_CRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
19-15 | PER_M | R | 1h | Internal. Only to be used through TI provided API. |
14-12 | PER_E | R | 4h | Internal. Only to be used through TI provided API. |
11-0 | RESERVED | R | 0h | Reserved |
CONFIG_IF_ADC is shown in Table 11-73.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | FF2ADJ | R | 3h | Internal. Only to be used through TI provided API. |
27-24 | FF3ADJ | R | 4h | Internal. Only to be used through TI provided API. |
23-20 | INT3ADJ | R | 6h | Internal. Only to be used through TI provided API. |
19-16 | FF1ADJ | R | 0h | Internal. Only to be used through TI provided API. |
15-14 | AAFCAP | R | 3h | Internal. Only to be used through TI provided API. |
13-10 | INT2ADJ | R | Dh | Internal. Only to be used through TI provided API. |
9-5 | IFDIGLDO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
4-0 | IFANALDO_TRIM_OUTPUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
CONFIG_OSC_TOP is shown in Table 11-74.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-30 | RESERVED | R | 0h | Reserved |
29-26 | XOSC_HF_ROW_Q12 | R | 7h | Internal. Only to be used through TI provided API. |
25-10 | XOSC_HF_COLUMN_Q12 | R | 1FFh | Internal. Only to be used through TI provided API. |
9-2 | RCOSCLF_CTUNE_TRIM | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
1-0 | RCOSCLF_RTUNE_TRIM | R | 0h | Internal. Only to be used through TI provided API. |
SOC_ADC_ABS_GAIN is shown in Table 11-75.
Return to the Summary Table.
AUX_ADC Gain in Absolute Reference Mode
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-0 | SOC_ADC_ABS_GAIN_TEMP1 | R | X | SOC_ADC gain in absolute reference mode at temperature
1 (30C). Calculated in production test.. Default value holds log information from production test. |
SOC_ADC_REL_GAIN is shown in Table 11-76.
Return to the Summary Table.
AUX_ADC Gain in Relative Reference Mode
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-0 | SOC_ADC_REL_GAIN_TEMP1 | R | X | SOC_ADC gain in relative reference mode at temperature
1 (30C). Calculated in production test.. Default value holds trim value from production test. |
SOC_ADC_OFFSET_INT is shown in Table 11-77.
Return to the Summary Table.
AUX_ADC Temperature Offsets in Absolute Reference Mode
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-24 | RESERVED | R | 0h | Reserved |
23-16 |
SOC_ADC_REL_ OFFSET_TEMP1 | R | X | SOC_ADC offset in relative reference mode at temperature 1 (30C). Signed 8-bit number. Calculated in production test.. Default value holds trim value from production test. |
15-8 | RESERVED | R | 0h | Reserved |
7-0 |
SOC_ADC_ABS_ OFFSET_TEMP1 | R | X | SOC_ADC offset in absolute reference mode at temperature 1 (30C). Signed 8-bit number. Calculated in production test.. Default value holds trim value from production test. |
SOC_ADC_REF_TRIM_AND_OFFSET_EXT is shown in Table 11-78.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-6 | RESERVED | R | 0h | Reserved |
5-0 | SOC_ADC_REF_VOLTAGE_TRIM_TEMP1 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
AMPCOMP_TH1 is shown in Table 11-79.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-24 | RESERVED | R | 0h | Reserved |
23-18 | HPMRAMP3_LTH | R | 1Eh | Internal. Only to be used through TI provided API. |
17-16 | RESERVED | R | 0h | Reserved |
15-10 | HPMRAMP3_HTH | R | 20h | Internal. Only to be used through TI provided API. |
9-6 |
IBIASCAP_LPTOHP_ OL_CNT | R | Ah | Internal. Only to be used through TI provided API. |
5-0 | HPMRAMP1_TH | R | Eh | Internal. Only to be used through TI provided API. |
AMPCOMP_TH2 is shown in Table 11-80.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-26 | LPMUPDATE_LTH | R | 1Ah | Internal. Only to be used through TI provided API. |
25-24 | RESERVED | R | 0h | Reserved |
23-18 | LPMUPDATE_HTM | R | 22h | Internal. Only to be used through TI provided API. |
17-16 | RESERVED | R | 0h | Reserved |
15-10 | ADC_COMP_AMPTH_LPM | R | 0h | Internal. Only to be used through TI provided API. |
9-8 | RESERVED | R | 0h | Reserved |
7-2 | ADC_COMP_AMPTH_HPM | R | 0h | Internal. Only to be used through TI provided API. |
1-0 | RESERVED | R | 0h | Reserved |
AMPCOMP_CTRL1 is shown in Table 11-81.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | RESERVED | R | 0h | Reserved |
30 | AMPCOMP_REQ_MODE | R | 1h | Internal. Only to be used through TI provided API. |
29-24 | RESERVED | R | 0h | Reserved |
23-20 | IBIAS_OFFSET | R | 4h | Internal. Only to be used through TI provided API. |
19-16 | IBIAS_INIT | R | 8h | Internal. Only to be used through TI provided API. |
15-8 |
LPM_IBIAS_WAIT_ CNT_FINAL | R | 3Fh | Internal. Only to be used through TI provided API. |
7-4 | CAP_STEP | R | 4h | Internal. Only to be used through TI provided API. |
3-0 |
IBIASCAP_HPTOLP_ OL_CNT | R | 7h | Internal. Only to be used through TI provided API. |
ANABYPASS_VALUE2 is shown in Table 11-82.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-14 | RESERVED | R | 0h | Reserved |
13-0 | XOSC_HF_IBIASTHERM | R | 3FFh | Internal. Only to be used through TI provided API. |
VOLT_TRIM is shown in Table 11-83.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-29 | RESERVED | R | 0h | Reserved |
28-24 | VDDR_TRIM_HH | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
23-21 | RESERVED | R | 0h | Reserved |
20-16 | VDDR_TRIM_H | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
15-13 | RESERVED | R | 0h | Reserved |
12-8 | VDDR_TRIM_SLEEP_H | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
7-5 | RESERVED | R | 0h | Reserved |
4-0 | TRIMBOD_H | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
OSC_CONF is shown in Table 11-84.
Return to the Summary Table.
OSC Configuration
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-30 | RESERVED | R | 0h | Reserved |
29 | ADC_SH_VBUF_EN | R | 1h | Trim value for DDI_0_OSC:ADCDOUBLERNANOAMPCTL.ADC_SH_VBUF_EN. |
28 | ADC_SH_MODE_EN | R | 1h | Trim value for DDI_0_OSC:ADCDOUBLERNANOAMPCTL.ADC_SH_MODE_EN. |
27 |
ATESTLF_RCOSCLF_ IBIAS_TRIM |
R | 0h | Trim value for DDI_0_OSC:ATESTCTL.ATESTLF_RCOSCLF_IBIAS_TRIM. |
26-25 |
XOSCLF_REGULATOR_ TRIM |
R | 0h | Trim value for DDI_0_OSC:LFOSCCTL.XOSCLF_REGULATOR_TRIM. |
24-21 |
XOSCLF_CMIRRWR_ RATIO |
R | 0h | Trim value for DDI_0_OSC:LFOSCCTL.XOSCLF_CMIRRWR_RATIO. |
20-19 | XOSC_HF_FAST_START | R | 1h | Trim value for DDI_0_OSC:CTL1.XOSC_HF_FAST_START. |
18 | XOSC_OPTION | R | X | 0: XOSC_HF unavailable (may not be bonded out) 1: XOSC_HF available (default) Default value differs depending on partnumber. |
17 | HPOSC_OPTION | R | X | Internal. Only to be used through TI provided API. Default value differs depending on partnumber. |
16 |
HPOSC_BIAS_HOLD_ MODE_EN |
R | 1h | Internal. Only to be used through TI provided API. |
15-12 |
HPOSC_CURRMIRR_ RATIO |
R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-8 | HPOSC_BIAS_RES_SET | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
7 | HPOSC_FILTER_EN | R | 1h | Internal. Only to be used through TI provided API. |
6-5 |
HPOSC_BIAS_RECHARGE _DELAY |
R | 3h | Internal. Only to be used through TI provided API. |
4-3 | RESERVED | R | 0h | Reserved |
2-1 | HPOSC_SERIES_CAP | R | 3h | Internal. Only to be used through TI provided API. |
0 | HPOSC_DIV3_BYPASS | R | 0h | Internal. Only to be used through TI provided API. |
FREQ_OFFSET is shown in Table 11-85.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | HPOSC_COMP_P0 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
15-8 | HPOSC_COMP_P1 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
7-0 | HPOSC_COMP_P2 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
MISC_OTP_DATA_1 is shown in Table 11-86.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-29 | RESERVED | R | 0h | Reserved |
28-27 | PEAK_DET_ITRIM | R | 0h | Internal. Only to be used through TI provided API. |
26-24 | HP_BUF_ITRIM | R | 0h | Internal. Only to be used through TI provided API. |
23-22 | LP_BUF_ITRIM | R | 2h | Internal. Only to be used through TI provided API. |
21-20 |
DBLR_LOOP_FILTER_ RESET_VOLTAGE | R | 0h | Internal. Only to be used through TI provided API. |
19-10 | HPM_IBIAS_WAIT_CNT | R | 100h | Internal. Only to be used through TI provided API. |
9-4 | LPM_IBIAS_WAIT_CNT | R | 3Fh | Internal. Only to be used through TI provided API. |
3-0 | IDAC_STEP | R | 8h | Internal. Only to be used through TI provided API. |
SHDW_DIE_ID_0 is shown in Table 11-87.
Return to the Summary Table.
Shadow of DIE_ID_0 register in eFuse
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | ID_31_0 | R | X | Shadow of DIE_ID_0 register in eFuse row number 5 Default value depends on eFuse value. |
SHDW_DIE_ID_1 is shown in Table 11-88.
Return to the Summary Table.
Shadow of DIE_ID_1 register in eFuse
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | ID_63_32 | R | X | Shadow of DIE_ID_1 register in eFuse row number 6 Default value depends on eFuse value. |
SHDW_DIE_ID_2 is shown in Table 11-89.
Return to the Summary Table.
Shadow of DIE_ID_2 register in eFuse
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | ID_95_64 | R | X | Shadow of DIE_ID_2 register in eFuse row number 7 Default value depends on eFuse value. |
SHDW_DIE_ID_3 is shown in Table 11-90.
Return to the Summary Table.
Shadow of DIE_ID_3 register in eFuse
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | ID_127_96 | R | X | Shadow of DIE_ID_3 register in eFuse row number 8 Default value depends on eFuse value. |
SHDW_SCAN_MCU3_SEC is shown in Table 11-91.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-24 | SECURITY | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
23 | RESERVED | R | 0h | Reserved |
22-11 | ULL_MCU_RAM_0_REP | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
10-0 | ULL_MCU_RAM_1_REP_1 | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
SHDW_SCAN_DATA1_CRC is shown in Table 11-92.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | FLASH_RDY | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
30-9 | RESERVED | R | 0h | Reserved |
8-1 | CRC | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
0 | TAP_DAP_LOCK_N | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
SHDW_ANA_TRIM is shown in Table 11-93.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | RESERVED | R | 0h | Reserved |
30 | ALT_VDDR_TRIM | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
29 | DET_LOGIC_DIS | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
28-27 | BOD_BANDGAP_TRIM_CNF_EXT | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
26-25 | BOD_BANDGAP_TRIM_CNF | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
24 | VDDR_ENABLE_PG1 | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
23 | VDDR_OK_HYS | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
22-21 | IPTAT_TRIM | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
20-16 | VDDR_TRIM | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
15-11 | TRIMBOD_INTMODE | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
10-6 | TRIMBOD_EXTMODE | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
5-0 | TRIMTEMP | R | X | Internal. Only to be used through TI provided API. Default value depends on eFuse value. |
OSC_CONF1 is shown in Table 11-94.
Return to the Summary Table.
Oscillator configuration
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 |
RCOSC_MF_BIAS_ HTEMP |
R | X | Defines the MF_BIAS trim code to use for high temp. Only valid if RCOSC_MF_SINGLE_TRIM_METHOD == 0 Default value holds trim value from production test. |
27 |
RCOSC_MF_TEMP_ DEPEND_MODE |
R | X | Defines whether dual trim was needed: 0: Dual trims needed on this chip 1: Dual trims not needed on this chip Default value holds trim value from production test. |
26 |
RCOSC_MF_SINGLE_ TRIM_METHOD |
R | X | Defines trim method used: 0: Dual trim method 1: Single trim method Default value holds trim value from production test. |
25-4 | RESERVED | R | 0h | Reserved |
3-0 | RCOSC_MF_BIAS_ADJ | R | X | Value is written to
DDI_0_OSC:RCOSCMFCTL.RCOSC_MF_BIAS_ADJ by boot FW while in
safezone. Default value holds trim value from production test. |
DAC_BIAS_CNF is shown in Table 11-95.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-18 | RESERVED | R | 0h | Reserved |
17-12 | LPM_TRIM_IOUT | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
11-9 | LPM_BIAS_WIDTH_TRIM | R | 0h | Internal. Only to be used through TI provided API. |
8 | LPM_BIAS_BACKUP_EN | R | 0h | Internal. Only to be used through TI provided API. |
7-0 | RESERVED | R | 0h | Reserved |
TFW_PROBE is shown in Table 11-96.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | REV | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
TFW_FT is shown in Table 11-97.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | REV | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
DAC_CAL0 is shown in Table 11-98.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 |
SOC_DAC_VOUT_CAL_ DECOUPLE_C2 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
15-0 |
SOC_DAC_VOUT_CAL_ DECOUPLE_C1 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
DAC_CAL1 is shown in Table 11-99.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 |
SOC_DAC_VOUT_CAL_ PRECH_C2 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
15-0 |
SOC_DAC_VOUT_CAL_ PRECH_C1 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
DAC_CAL2 is shown in Table 11-100.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 |
SOC_DAC_VOUT_CAL_ ADCREF_C2 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
15-0 |
SOC_DAC_VOUT_CAL_ ADCREF_C1 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
DAC_CAL3 is shown in Table 11-101.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 |
SOC_DAC_VOUT_CAL_ VDDS_C2 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |
15-0 |
SOC_DAC_VOUT_CAL_ VDDS_C1 | R | X | Internal. Only to be used through TI provided API. Default value holds trim value from production test. |