SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
Table 8-3 lists the memory-mapped registers for the FLASH registers. All register offset addresses not listed in Table 8-3 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Section |
---|---|---|---|
0h | WEPROT_B0_31_0_BY1 | Internal | Section 8.6.1.1 |
4h | WEPROT_AUX_BY1 | Internal | Section 8.6.1.2 |
1Ch | STAT | NW and Efuse Status | Section 8.6.1.3 |
24h | CFG | Internal | Section 8.6.1.4 |
2Ch | FLASH_SIZE | Internal | Section 8.6.1.5 |
3Ch | FWLOCK | Internal | Section 8.6.1.6 |
40h | FWFLAG | Internal | Section 8.6.1.7 |
50h | BANK0_TRIM_CFG_3 | Internal | Section 8.6.1.8 |
54h | BANK0_TRIM_CFG_2 | Internal | Section 8.6.1.9 |
58h | BANK0_TRIM_CFG_1 | Internal | Section 8.6.1.10 |
5Ch | BANK0_TRIM_CFG_0 | Internal | Section 8.6.1.11 |
60h | BANK1_TRIM_CFG_3 | Internal | Section 8.6.1.12 |
64h | BANK1_TRIM_CFG_2 | Internal | Section 8.6.1.13 |
68h | BANK1_TRIM_CFG_1 | Internal | Section 8.6.1.14 |
6Ch | BANK1_TRIM_CFG_0 | Internal | Section 8.6.1.15 |
70h | PUMP_TRIM_CFG_2 | Internal | Section 8.6.1.16 |
74h | PUMP_TRIM_CFG_1 | Internal | Section 8.6.1.17 |
78h | PUMP_TRIM_CFG_0 | Internal | Section 8.6.1.18 |
1000h | EFUSE | Internal | Section 8.6.1.19 |
1004h | EFUSEADDR | Internal | Section 8.6.1.20 |
1008h | DATAUPPER | Internal | Section 8.6.1.21 |
100Ch | DATALOWER | Internal | Section 8.6.1.22 |
1010h | EFUSECFG | Internal | Section 8.6.1.23 |
1014h | EFUSESTAT | Internal | Section 8.6.1.24 |
1018h | ACC | Internal | Section 8.6.1.25 |
101Ch | BOUNDARY | Internal | Section 8.6.1.26 |
1020h | EFUSEFLAG | Internal | Section 8.6.1.27 |
1024h | EFUSEKEY | Internal | Section 8.6.1.28 |
1028h | EFUSERELEASE | Internal | Section 8.6.1.29 |
102Ch | EFUSEPINS | Internal | Section 8.6.1.30 |
1030h | EFUSECRA | Internal | Section 8.6.1.31 |
1034h | EFUSEREAD | Internal | Section 8.6.1.32 |
1038h | EFUSEPROGRAM | Internal | Section 8.6.1.33 |
103Ch | EFUSEERROR | Internal | Section 8.6.1.34 |
1040h | SINGLEBIT | Internal | Section 8.6.1.35 |
1044h | TWOBIT | Internal | Section 8.6.1.36 |
1048h | SELFTESTCYC | Internal | Section 8.6.1.37 |
104Ch | SELFTESTSIGN | Internal | Section 8.6.1.38 |
Complex bit access types are encoded to fit into small table cells. Table 8-4 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
Write Type | ||
W | W | Write |
Reset or Default Value | ||
-n | Value after reset or the default value |
WEPROT_B0_31_0_BY1 is shown in Table 8-5.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | WEPROT_B0_31_0_BY1 | R/W | FFFFFFFFh | Internal. Only to be used through TI provided API. |
WEPROT_AUX_BY1 is shown in Table 8-6.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-6 | RESERVED | R | 0h | Reserved |
5 | WEPROT_B1_ENGR_BY1 | R/W | 1h | Internal. Only to be used through TI provided API. |
4 | WEPROT_B0_ENGR_BY1 | R/W | 1h | Internal. Only to be used through TI provided API. |
3 | WEPROT_B1_TRIM_BY1 | R/W | 1h | Internal. Only to be used through TI provided API. |
2 | WEPROT_B0_TRIM_BY1 | R/W | 1h | Internal. Only to be used through TI provided API. |
1 | WEPROT_B1_FCFG_BY1 | R/W | 1h | Internal. Only to be used through TI provided API. |
0 | WEPROT_B0_CCFG_BY1 | R/W | 1h | Internal. Only to be used through TI provided API. |
STAT is shown in Table 8-7.
Return to the Summary Table.
NW and Efuse Status
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-17 | RESERVED | R | 0h | Reserved |
16 | STALLSTAT | R/W | 0h | An ocp1 or ocp3 read stall has occurred. 0 : No stall or stall acknowledged by writing a 1 1 : Stall condition occurred/occurring This is a read/write-clear status bit. It will reset to 0. It will be set when either an ocp1 or ocp3 read occurs to a bank that is presently undergoing a program or write operation. An ocp2 write of 1 to this bit will clear the bit. The ocp2 write will take highest priority in the event an ocp1/ocp3 read is occurring concurrently to the ocp2 write. Clearing the bit should be done only after the ongoing program/erase operation is complete indicating that both banks are free. If clearing occurs while the stall condition persists, the field may get set back to one. |
15 | EFUSE_BLANK | R | 0h | Efuse scanning detected if fuse ROM is blank: 0 : Not blank 1 : Blank |
14 | EFUSE_TIMEOUT | R | 0h | Efuse scanning resulted in timeout error. 0 : No Timeout error 1 : Timeout Error |
13 | SPRS_BYTE_NOT_OK | R | 0h | Efuse scanning resulted in scan chain Sparse byte
error. 0 : No Sparse error 1 : Sparse Error |
12-8 | EFUSE_ERRCODE | R | 0h | Same as EFUSEERROR.CODE |
7-6 | RESERVED | R | 0h | Software should not rely on the value of a reserved bit. To provide compatibility with future products, the value of a reserved bit should be preserved across a read-modify-write operation |
5-4 | BUSY | R | 0h | NW FW_SMSTAT.CMD_IN_PROGRESS bit. This flag is valid immediately after the operation setting it 0 : Not busy 1 : Busy Bit 4 is for the busy state for Bank0 which is at logical address 0x0 Bit 5 for Bank1. |
3 | READY1T | R | 0h | 1T access readiness status indicator from NW. Comes
later than 2T readiness. 1: FLASH banks are ready for 1T accesses 0: FLASH banks are not ready for 1T accesses |
2 | READY2T | R | 0h | 2T access readiness status indicator from NW 1: FLASH banks are ready for 2T accesses 0: FLASH banks are not ready for 2T accesses |
1-0 | POWER_MODE | R | 0h | Power state of each of the 2 flash arbiter FSM
instances in the flash sub-system. For Thor, these bits should
mostly be in the same state since both banks are in the same power
mode. 0 : Active 1 : Ready for Low power (The 2T readiness has gone low or the flash_off_req has been set=1, and flash_off_ack is ready to be asserted). Bit 0 is for the power state for Bank0 which is at logical address 0x0 Bit 1 for Bank1 |
CFG is shown in Table 8-8.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | RESERVED | R | 0h | Reserved |
30 | DIS_FWTEST | R/W | 0h | Internal. Only to be used through TI provided API. |
29-12 | RESERVED | R | 0h | Reserved |
11 | MAIN_STICKY_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
10 | CCFG_STICKY_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
9 | FCFG_STICKY_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
8 | ENGR_TRIM_STICKY_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
7-6 | RESERVED | R | 0h | Reserved |
5 | DIS_EFUSECLK | R/W | 0h | Internal. Only to be used through TI provided API. |
4 | DIS_READACCESS | R/W | 0h | Internal. Only to be used through TI provided API. |
3-1 | RESERVED | R | 0h | Reserved |
0 | BP_TRIMCFG_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
FLASH_SIZE is shown in Table 8-9.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-10 | RESERVED | R | 0h | Reserved |
9-7 | SECTORS | R/W | 4h | Internal. Only to be used through TI provided API. |
6-0 | RESERVED | R | 0h | Internal. Only to be used through TI provided API. |
FWLOCK is shown in Table 8-10.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-3 | RESERVED | R | 0h | Reserved |
2-0 | FWLOCK | R/W | 0h | Internal. Only to be used through TI provided API. |
FWFLAG is shown in Table 8-11.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-3 | RESERVED | R | 0h | Reserved |
2-0 | FWFLAG | R/W | 0h | Internal. Only to be used through TI provided API. |
BANK0_TRIM_CFG_3 is shown in Table 8-12.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | RESERVED | R | 0h | Reserved |
BANK0_TRIM_CFG_2 is shown in Table 8-13.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | RESERVED | R | 0h | Reserved |
BANK0_TRIM_CFG_1 is shown in Table 8-14.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | RESERVED | R | 0h | Reserved |
27-22 | REDSWSELW3 | R/W | 0h | Internal. Only to be used through TI provided API. |
21-16 | REDSWSELW2 | R/W | 0h | Internal. Only to be used through TI provided API. |
15-10 | REDSWSELW1 | R/W | 0h | Internal. Only to be used through TI provided API. |
9-4 | REDSWSELW0 | R/W | 0h | Internal. Only to be used through TI provided API. |
3 | REDSWENW3 | R/W | 0h | Internal. Only to be used through TI provided API. |
2 | REDSWENW2 | R/W | 0h | Internal. Only to be used through TI provided API. |
1 | REDSWENW1 | R/W | 0h | Internal. Only to be used through TI provided API. |
0 | REDSWENW0 | R/W | 0h | Internal. Only to be used through TI provided API. |
BANK0_TRIM_CFG_0 is shown in Table 8-15.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | BANK0_TRIM_CFG_0 | R/W | 0h | Internal. Only to be used through TI provided API. |
BANK1_TRIM_CFG_3 is shown in Table 8-16.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | RESERVED | R | 0h | Reserved |
BANK1_TRIM_CFG_2 is shown in Table 8-17.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | RESERVED | R | 0h | Reserved |
BANK1_TRIM_CFG_1 is shown in Table 8-18.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | RESERVED | R | 0h | Reserved |
27-22 | REDSWSELW3 | R/W | 0h | Internal. Only to be used through TI provided API. |
21-16 | REDSWSELW2 | R/W | 0h | Internal. Only to be used through TI provided API. |
15-10 | REDSWSELW1 | R/W | 0h | Internal. Only to be used through TI provided API. |
9-4 | REDSWSELW0 | R/W | 0h | Internal. Only to be used through TI provided API. |
3 | REDSWENW3 | R/W | 0h | Internal. Only to be used through TI provided API. |
2 | REDSWENW2 | R/W | 0h | Internal. Only to be used through TI provided API. |
1 | REDSWENW1 | R/W | 0h | Internal. Only to be used through TI provided API. |
0 | REDSWENW0 | R/W | 0h | Internal. Only to be used through TI provided API. |
BANK1_TRIM_CFG_0 is shown in Table 8-19.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | BANK1_TRIM_CFG_0 | R/W | 0h | Internal. Only to be used through TI provided API. |
PUMP_TRIM_CFG_2 is shown in Table 8-20.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-26 | RESERVED | R | 0h | Reserved |
25-20 | VWLCT | R/W | 5h | Internal. Only to be used through TI provided API. |
19-14 | VSLCT | R/W | 16h | Internal. Only to be used through TI provided API. |
13-9 | VREADCT | R/W | Ah | Internal. Only to be used through TI provided API. |
8-4 | VINLOWCCORCT | R/W | 0h | Internal. Only to be used through TI provided API. |
3-0 | VINHICCORCT | R/W | 0h | Internal. Only to be used through TI provided API. |
PUMP_TRIM_CFG_1 is shown in Table 8-21.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | VINHICCORCTLSB | R/W | 0h | Internal. Only to be used through TI provided API. |
30-25 | VINHCT | R/W | Ch | Internal. Only to be used through TI provided API. |
24-20 | VCGCT | R/W | 12h | Internal. Only to be used through TI provided API. |
19-15 | IREFVRDCT | R/W | 0h | Internal. Only to be used through TI provided API. |
14-10 | IREFTCCT | R/W | 0h | Internal. Only to be used through TI provided API. |
9-6 | IREFCT | R/W | 0h | Internal. Only to be used through TI provided API. |
5-0 | FOSCCT | R/W | 0h | Internal. Only to be used through TI provided API. |
PUMP_TRIM_CFG_0 is shown in Table 8-22.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-30 | RESERVED | R | 0h | Reserved |
29-20 | VHVCT_PV | R/W | Bh | Internal. Only to be used through TI provided API. |
19-10 | VHVCT_PGM | R/W | 131h | Internal. Only to be used through TI provided API. |
9-0 | VHVCT_ERS | R/W | 13Ah | Internal. Only to be used through TI provided API. |
EFUSE is shown in Table 8-23.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-29 | RESERVED | R | 0h | Reserved |
28-24 | INSTRUCTION | R/W | 0h | Internal. Only to be used through TI provided API. |
23-16 | RESERVED | R | 0h | Reserved |
15-0 | DUMPWORD | R/W | 0h | Internal. Only to be used through TI provided API. |
EFUSEADDR is shown in Table 8-24.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-11 | BLOCK | R/W | 0h | Internal. Only to be used through TI provided API. |
10-0 | ROW | R/W | 0h | Internal. Only to be used through TI provided API. |
DATAUPPER is shown in Table 8-25.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-3 | SPARE | R/W | 0h | Internal. Only to be used through TI provided API. |
2 | P | R/W | 0h | Internal. Only to be used through TI provided API. |
1 | R | R/W | 0h | Internal. Only to be used through TI provided API. |
0 | EEN | R/W | 0h | Internal. Only to be used through TI provided API. |
DATALOWER is shown in Table 8-26.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | DATA | R/W | 0h | Internal. Only to be used through TI provided API. |
EFUSECFG is shown in Table 8-27.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-9 | RESERVED | R | 0h | Reserved |
8 | IDLEGATING | R/W | 0h | Internal. Only to be used through TI provided API. |
7-5 | RESERVED | R | 0h | Reserved |
4-3 | SLAVEPOWER | R/W | 0h | Internal. Only to be used through TI provided API. |
2-1 | RESERVED | R | 0h | Reserved |
0 | GATING | R/W | 1h | Internal. Only to be used through TI provided API. |
EFUSESTAT is shown in Table 8-28.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-1 | RESERVED | R | 0h | Reserved |
0 | RESETDONE | R | 1h | Internal. Only to be used through TI provided API. |
ACC is shown in Table 8-29.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-24 | RESERVED | R | 0h | Reserved |
23-0 | ACCUMULATOR | R | 0h | Internal. Only to be used through TI provided API. |
BOUNDARY is shown in Table 8-30.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-24 | RESERVED | R | 0h | Reserved |
23 | DISROW0 | R/W | 0h | Internal. Only to be used through TI provided API. |
22 | SPARE | R/W | 0h | Internal. Only to be used through TI provided API. |
21 | EFC_SELF_TEST_ERROR | R/W | 0h | Internal. Only to be used through TI provided API. |
20 | EFC_INSTRUCTION_INFO | R/W | 0h | Internal. Only to be used through TI provided API. |
19 | EFC_INSTRUCTION_ERROR | R/W | 0h | Internal. Only to be used through TI provided API. |
18 | EFC_AUTOLOAD_ERROR | R/W | 0h | Internal. Only to be used through TI provided API. |
17-14 | OUTPUTENABLE | R/W | 0h | Internal. Only to be used through TI provided API. |
13 | SYS_ECC_SELF_TEST_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
12 | SYS_ECC_OVERRIDE_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
11 | EFC_FDI | R/W | 0h | Internal. Only to be used through TI provided API. |
10 | SYS_DIEID_AUTOLOAD_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
9-8 | SYS_REPAIR_EN | R/W | 0h | Internal. Only to be used through TI provided API. |
7-4 | SYS_WS_READ_STATES | R/W | 0h | Internal. Only to be used through TI provided API. |
3-0 | INPUTENABLE | R/W | 0h | Internal. Only to be used through TI provided API. |
EFUSEFLAG is shown in Table 8-31.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-1 | RESERVED | R | 0h | Reserved |
0 | KEY | R | 0h | Internal. Only to be used through TI provided API. |
EFUSEKEY is shown in Table 8-32.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | CODE | R/W | 0h | Internal. Only to be used through TI provided API. |
EFUSERELEASE is shown in Table 8-33.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-25 | ODPYEAR | R | X | Internal. Only to be used through TI provided API. |
24-21 | ODPMONTH | R | X | Internal. Only to be used through TI provided API. |
20-16 | ODPDAY | R | X | Internal. Only to be used through TI provided API. |
15-9 | EFUSEYEAR | R | X | Internal. Only to be used through TI provided API. |
8-5 | EFUSEMONTH | R | X | Internal. Only to be used through TI provided API. |
4-0 | EFUSEDAY | R | X | Internal. Only to be used through TI provided API. |
EFUSEPINS is shown in Table 8-34.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Internal. Only to be used through TI provided API. |
15 | EFC_SELF_TEST_DONE | R | X | Internal. Only to be used through TI provided API. |
14 | EFC_SELF_TEST_ERROR | R | X | Internal. Only to be used through TI provided API. |
13 | SYS_ECC_SELF_TEST_EN | R | X | Internal. Only to be used through TI provided API. |
12 | EFC_INSTRUCTION_INFO | R | X | Internal. Only to be used through TI provided API. |
11 | EFC_INSTRUCTION_ERROR | R | X | Internal. Only to be used through TI provided API. |
10 | EFC_AUTOLOAD_ERROR | R | X | Internal. Only to be used through TI provided API. |
9 | SYS_ECC_OVERRIDE_EN | R | X | Internal. Only to be used through TI provided API. |
8 | EFC_READY | R | X | Internal. Only to be used through TI provided API. |
7 | EFC_FCLRZ | R | X | Internal. Only to be used through TI provided API. |
6 | SYS_DIEID_AUTOLOAD_EN | R | X | Internal. Only to be used through TI provided API. |
5-4 | SYS_REPAIR_EN | R | X | Internal. Only to be used through TI provided API. |
3-0 | SYS_WS_READ_STATES | R | X | Internal. Only to be used through TI provided API. |
EFUSECRA is shown in Table 8-35.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-6 | RESERVED | R | 0h | Reserved |
5-0 | DATA | R/W | 0h | Internal. Only to be used through TI provided API. |
EFUSEREAD is shown in Table 8-36.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-10 | RESERVED | R | 0h | Reserved |
9-8 | DATABIT | R/W | 0h | Internal. Only to be used through TI provided API. |
7-4 | READCLOCK | R/W | 0h | Internal. Only to be used through TI provided API. |
3 | DEBUG | R/W | 0h | Internal. Only to be used through TI provided API. |
2 | SPARE | R/W | 0h | Internal. Only to be used through TI provided API. |
1-0 | MARGIN | R/W | 0h | Internal. Only to be used through TI provided API. |
EFUSEPROGRAM is shown in Table 8-37.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | RESERVED | R | 0h | Reserved |
30 | COMPAREDISABLE | R/W | 0h | Internal. Only to be used through TI provided API. |
29-14 | CLOCKSTALL | R/W | 0h | Internal. Only to be used through TI provided API. |
13 | VPPTOVDD | R/W | 0h | Internal. Only to be used through TI provided API. |
12-9 | ITERATIONS | R/W | 0h | Internal. Only to be used through TI provided API. |
8-0 | WRITECLOCK | R/W | 0h | Internal. Only to be used through TI provided API. |
EFUSEERROR is shown in Table 8-38.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-6 | RESERVED | R | 0h | Reserved |
5 | DONE | R/W | 0h | Internal. Only to be used through TI provided API. |
4-0 | CODE | R/W | 0h | Internal. Only to be used through TI provided API. |
SINGLEBIT is shown in Table 8-39.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-1 | FROMN | R | 0h | Internal. Only to be used through TI provided API. |
0 | FROM0 | R | 0h | Internal. Only to be used through TI provided API. |
TWOBIT is shown in Table 8-40.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-1 | FROMN | R | 0h | Internal. Only to be used through TI provided API. |
0 | FROM0 | R | 0h | Internal. Only to be used through TI provided API. |
SELFTESTCYC is shown in Table 8-41.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | CYCLES | R/W | 0h | Internal. Only to be used through TI provided API. |
SELFTESTSIGN is shown in Table 8-42.
Return to the Summary Table.
Internal. Only to be used through TI provided API.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | SIGNATURE | R/W | 0h | Internal. Only to be used through TI provided API. |