SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
The procedure takes the following input parameter:
The procedure returns the following:
The procedure returns with error if the specified queue is empty. Otherwise, the following is done:
set pTemp = pQueue->pCurrEntry
set pQueue->pCurrEntry = pTemp->pNextEntry
set pTemp->status = Finished
set pEntry = pQueue->pCurrEntry