SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
The Sensor Controller can leverage the MAC module for mathematical operations, such as:
The results from these operations are always stored in the 40-bit signed accumulator. The Sensor Controller can perform the following operations directly on the accumulator:
Figure 20-7 shows a block diagram of the MAC.
For consistent timing, it is important that the Sensor Controller and the MAC operational rates are equal. Hence, the Sensor Controller application must set the MAC_OP_RATE bit of the AUX_SYSIF:PEROPRATE register to SCE_RATE (see Section 20.8.9).
Though not the primary use case, the System CPU can also use the MAC. To achieve consistent timing in this case, the application must set the MAC_OP_RATE bit of the AUX_SYSIF:PEROPRATE register to BUS_RATE (see Section 20.8.9).
The result of addition and multiplication operations is still valid if operations are unequal, but the time to complete the operations can vary.
The addition and multiplication operations require multiple peripheral clock cycles to complete. Consider the following assembly example that was generated from the Sensor Controller Studio.
# Sample assembly (Example code produced by the Sensor Controller Studio)
# The contents of r4 are assumed to be signed in this example
0: out R4,[#IOP_MAC_OP1SADD16] ; add r4 to the accumulator
1: in R1,[#IOP_MAC_15_0] ; Store result bits 15:0 in r1
2: out R4,[#IOP_MAC_OP1SMUL] ; Multiply r4 with operand 0(assumed pre-programmed)
3: in R2,[#IOP_MAC_31_16] ; Store result bits 31:16 in r2
4: in R3,[#IOP_MAC_15_0] ; Store result bits 15:0 in r3
# The Sensor Controller uses the alias I/O memory space
IOP_MAC_OP1SMUL equ 11
IOP_MAC_OP1SADD16 equ 15
IOP_MAC_31_16 equ 24
IOP_MAC_15_0 equ 23
As shown in Figure 20-8, the addition operation requires one peripheral clock cycle to complete. Because the Sensor Controller attempts to read the result of the operation immediately after triggering it, the Sensor Controller stalls for one clock cycle. This condition gates the clock to the Sensor Controller until the result is ready.
Figure 20-8 also shows that the multiplication operation requires five peripheral clock cycles to complete. As the Sensor Controller tries to read the result of the operation immediately after triggering it, the Sensor Controller stalls for five clock cycles. The clock to the Sensor Controller becomes clock gated until the result is ready. The multiply-accumulate operation requires the same number of peripheral clock cycles to complete.