SWPB019E April 2017 – August 2024 TMS320F280049-Q1 , TMS320F2802-Q1 , TMS320F28027 , TMS320F28027-Q1 , TMS320F28035 , TMS320F28035-Q1 , TMS320F28055 , TMS320F2806-Q1 , TMS320F28069 , TMS320F28069-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28333 , TMS320F28335 , TMS320F28335-Q1 , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1
The TI C2000™ F28x family of microcontrollers is designed for real-time control applications in both industrial and automotive spaces. All F28x microcontrollers feature 32-bit C28x CPUs, with speeds from 40MHz to 200MHz, often paired with accelerator cores such as the Control Law Accelerator (CLA). With tightly coupled analog peripherals such as analog-to-digital converters (ADCs), comparators, and sophisticated digital actuation peripherals, such as high resolution PWM modules, there are many compelling reasons to use C2000 microcontrollers in embedded real-time control applications.
C2000™ MCU Series |
Security Enablers |
Detailed Security Features |
---|---|---|
F28P55x+ F28P65x+ F280015x+ F280013x+ F28003x+ F28002x+ F2838x+ F28004x+ F2837xD+ F2837xS+ F2807x+ F2806x F2805x F2803x F2802x F2833x, F2823x F28M3x |
Device identification | Unique Identification (UID) Number: Ability for user to enable mechanisms for device identification in communications, seed for data integrity algorithms, initialization vector for authentication and encryption or decryption, or to protect against code cloning. |
Software IP protection | Code Security Module (CSM): Ability for user to block unauthorized access or programming of firmware stored in on-chip memories. Devices marked with (+) feature a Dual Code Security Module (DCSM), with two independent security zones. | |
Debug security | Emulation Code Security Logic (ECSL) using CSM: Ability for user to enable full debug access to memory using a password. |
C2000™ MCU Series |
Security Enablers | Detailed Security Features |
---|---|---|
F28P55x F28P65x F280015x F280013x F28003x F2838x |
Additional Debug Security | JTAGLOCK: Ability to block debugger access to the device; unlockable with password. |
Secure Boot | Option to enable AES-128 Cipher-based Message Authentication Code (CMAC) to pre-authenticate the first 16KB of flash prior to transferring code execution. | |
F28P55x F28P65x F28003x F2838x |
Cryptographic Acceleration | Hardware Advanced Encryption Standard (AES 128-, 192-, 256 bit) engine to boost performance. |
F28P55x | Flash write and erase protection | Option to permanently lock sections of Flash, making the contents immutable. This can be used to extend secure boot capabilities by implementing additional cryptographic functions in software for code and data authentication. |
In the design of real-time control systems, a good portion of the research and development investment goes into embedded firmware development. As such, intellectual property housed in the firmware of a product can provide key competitive advantages for users, and can be vulnerable to theft. Performing a visual component tear-down of a system is relatively easy for the purpose of replicating the end product, but effective protection of the firmware running on the MCU prevents full duplication of the working system.
Another scenario that is increasingly common is co-development of the firmware. In these cases, certain portions of system firmware are developed outside the core engineering team, and perhaps by a third party vendor. In these situations, one party can opt to keep the firmware private, while still allowing the second party to develop and test a portion of the application on the same system. Such scenarios are typically not covered by traditional runtime software protections, and require hardware protection mechanisms while the MCU is being accessed by a debugger.
This scenario is especially common in automotive applications, where there can be multiple companies involved in producing and debugging firmware in a highly connected system. These types of threats can be addressed by the security enablers available on C2000 devices.
When a new device is shipped from TI, the device arrives in a completely unlocked state. After security protocols are enabled by the user, any locked memory zone is only accessible by code that also exists in the same zone. Dedicated unlocked memory is available so that data can be transferred between zones if needed. In addition to this fundamental building block, there are other options or layers that can be selectively enabled:
In many cases, not all the memory, either volatile or nonvolatile, needs to be locked. This case can be true for certain pieces of firmware shared across different sub-systems, or that contain non-proprietary IP.
In addition to protecting various blocks of memory, there are two zones in each DCSM implementation. Once the memories are allocated for protection, the next step is deciding which of these zones has control over the selected memories. However, if there is no need for code protection between developers on the same device, a single-zone configuration can be used.
If a region is used only for execution, rather than internal data storage, the programmer can enable execute-only protection to block any read access (even from the same region or zone), for added security.
Debug access to the core processing unit (CPU) registers is also blocked if the DCSM detects code executing from any locked region.
Even with the above measures, users can restrict an emulation connection if the MCU is executing from a locked region. This security feature can be temporarily disabled during a debug session using a password.
By using a UID number provided on each device, techniques can be implemented to further allow software to only run on known devices. For more information, see C2000™ Unique Device Number.
The JTAG (emulator) interface can be disabled and protected with a user-chosen password. This helps make sure only authorized individuals can view and debug the application.
The widely used AES symmetric cipher is known for speed and simplicity. Even given that, a software implementation of the AES algorithm in an embedded microcontroller is relatively slow to the demands of a real-time control system. The hardware AES accelerator vastly improves processing time for cryptographic messages, while freeing up the CPU bandwidth in the process. Several different operational modes and key sizes are available.
To maintain the integrity of firmware stored in the device, secure boot can be enabled to verify code stored in Flash memory before transferring execution to the stored code. Along with the firmware programming protections built into the security logic, this helps make sure the code that runs on the device is authentic. The algorithm used is an AES-128 CMAC algorithm. Tools are available to embed the required MAC value into the final code image. For more information, see Secure Boot on C2000 Device.
In certain cases, users can opt to extend secure boot functionality by implementing other cryptographic authentication algorithms, including elliptic curve-based functions such as ECDSA. In devices with Flash write and erase protection, these functions can be placed in Flash regions at the entry point of code, and made immutable (that is, permanently unchangeable and unmodifiable). This feature enables stronger cryptographic capabilities, and can also be used to enable secure firmware update functions.
While security risks can take many forms across end applications, firmware intellectual property protection is a threat common to most systems. C2000 microcontrollers enable users to address these concerns through flexible features for multiuser development environments. For more information on C2000 microcontrollers, see TI.com/C2000. For specific information on the security features present in each C2000 device, see the product data sheet and technical reference manual available on the TI.COM™ product page.
For more information about TI’s Embedded Security Designs, visit TI.com/security.