SWRA491A September 2015 – October 2016 CC2640 , CC2640R2F , CC2650 , CC2650MODA
Advertising is used for four different purposes, regardless of the operation mode. Properties of each type of the ADVs used in this implementation are summarized in Table 2.
UID/URL/TLM Frame | URL Configuration Mode ADV | |
---|---|---|
ADV Event Type | ADV_NONCONN_IND | ADV_IND |
ADV Type Flags | BREDR_NOT_SUPPORTED | BREDR_NOT_SUPPORTED | GENERAL_DISCOVERABLE |
ADV Interval | From URL Cfg for UID/URL, 10 times longer for TLM | Default Interval |
TX Power | From URL Cfg | Medium Power Mode |
Connectable | No | Yes |
As switching from one advertising packet to another at run time is required, how to set the parameters to change the properties for regular advertising mode is described in this section. How to get the information to populate the payload of each packet is also covered.