SWRA536 February 2016 CC2520 , CC2520 , CC2530 , CC2530 , CC2530-RF4CE , CC2530-RF4CE , CC2533 , CC2533 , CC2540 , CC2540 , CC2541 , CC2541 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2640R2L , CC2640R2L , CC2650 , CC2650 , CC2650MODA , CC2650MODA
This application report describes the setup and procedure used to measure the new ETSI EN receiver (RX) blocking test added to version v2.1.1 of the ETSI EN 300 328 harmonized standard.
Project collateral discussed in this application report can be downloaded from the following URL: http://www.ti.com/lit/zip/swra536.
SmartRF is a trademark of Texas Instruments.
Bluetooth is a registered trademark of Bluetooth SIG, Inc.
Wi-Fi is a registered trademark of Wi-Fi Alliance.
ZigBee is a registered trademark of ZigBee Alliance.
All other trademarks are the property of their respective owners.
ETSI EN 300 328 is a European harmonized standard that specifies the regulatory requirement for data transmission equipment operating in the 2.4 GHz ISM band and using wide band modulation techniques in Europe. This standard covers technology such as Wi-Fi®, Bluetooth and ZigBee® but also other proprietary transmission systems that use the 2.4 GHz ISM band.
In the current version of V2.1.1, which was released in November, 2016 under the European Radio Equipment Directive 2014/53/EU (RED), a new requirement regarding receiver blocking performance was added and this application report shows how it can be measured for a Bluetooth low energy system using a Rohde & Schwartz vector signal generator. The same method can be applied for most other transmission systems or signal generator vendors.
The ETSI specification divides receivers into three different categories: category 1 to category 3. The categorization can be found in the Categorization section in the ETSI specification (V2.1.1, 2016, p.15). Bluetooth low energy devices fall in either category 2 or category 3 based on Medium Utilization (MU), a product of TX duty cycle and output power. Category 2 covers devices with output power between 0 and 10 dBm assuming 100% duty cycle, and has stricter requirements than category 3. As the CC2640 easily fulfills the requirements for category 2, we will only focus on these requirements throughout this document.
The blocking requirements for receiver category 2 is found in the Receiver Category 2 section in the ETSI specification (V2.1.1, 2016, p. 38).
Wanted Signal Mean Power
From Companion Device (dBm) |
Blocking Signal Frequency (MHz) | Blocking SIgnal Power (dBm)
(see (2)) |
Type of Blocking Signal |
---|---|---|---|
Pmin + 6 dB
(see (1)) |
2380
2503.5 |
-57 | CW |
Pmin + 6 dB
(see (1)) |
2300
2583.5 |
-47 | CW |
Tests should be performed at both lowest and highest operating frequency according to the Test Conditions section in the ETSI specification (V2.1.1, 2016, p. 72).