• Menu
  • Product
  • Email
  • PDF
  • Order now
  • AWR2243 Cascade

    • SWRA574B October   2017  – February 2020 AWR1243 , AWR2243

       

  • CONTENTS
  • SEARCH
  • AWR2243 Cascade
  1.   AWR2243 Cascade
    1.     Trademarks
    2. 1 Cascaded AWR2243 System
    3. 2 Synchronization of AWR2243 Chips
      1. 2.1 20 GHz (FMCW) RF LO Sync
      2. 2.2 Digital Frame Sync
        1. 2.2.1 Frame (Burst) and Chirp Timing in AWR2243
        2. 2.2.2 Frame (Burst) and Chirp Timing in a Cascaded System
        3. 2.2.3 Inter Chip Imbalance of Digital Sync Timing
      3. 2.3 40 MHz (System) Reference Clock Synchronization
    4. 3 Connectivity
      1. 3.1 20 GHz LO Sync Pins Connectivity
      2. 3.2 DIG_SYNC Connectivity
      3. 3.3 40 MHz (System) Reference Clock Connectivity
    5. 4 20 GHz LO Sync Link Budget
    6. 5 Software Messaging
      1. 5.1 Configuration of Devices
      2. 5.2 Configuration of Frames
        1. 5.2.1 Similar Configuration Across AWR2243 Devices
        2. 5.2.2 Dissimilar Configuration Across AWR2243 Devices
      3. 5.3 Triggering of Frames
      4. 5.4 Example Usage
      5. 5.5 Other Usages
    7. 6 Advantages of AWR2243 Cascading System
    8. 7 References
  2.   Revision History
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

AWR2243 Cascade

AWR2243 Cascade

This application report describes TI’s cascaded mmWave radar system. This solution is based on TI’s AWR2243 radar chip. Using the 20 GHz LO input and output paths, several of these chips are cascaded together and operated synchronously. Each AWR2243 chip supports up to four receive and three transmit antennas. Cascading multiple such chips allows the radar system to operate with more receive and transmit antennas, thereby improving target detection and resolution in comparison with a single AWR2243 radar chip based system. Cascading of two and four AWR2243 chips is illustrated in this application report. This cascaded radar solution is intended to support automotive applications such as Adaptive Cruise Control, Collision Warning, Emergency Braking, and Semi and Fully Autonomous Driving. The system described in this document has been implemented for evaluation in the mmWave cascade imaging radar RF evaluation module (https://www.ti.com/tool/MMWCAS-RF-EVM).

Trademarks

All other trademarks are the property of their respective owners.

1 Cascaded AWR2243 System

Multiple AWR2243 chips may be cascaded on PCB to improve target detection and resolution. In this section, two chip cascading and four chip cascading systems are illustrated as examples. The focus is on connection of various signals that the AWR2243 chips need to share among themselves. Of the multiple AWR2243 chips in the cascaded system, one is referred to as the Master and the others as Slaves. To make the entire cascaded system operate as a single radar system, the Master is designated to generate a common Local Oscillator (LO) signal (19 GHz to 20.25 GHz) shared across all the transmitters and receivers in the entire cascade system. The master also controls the radar chirp/frame timing for all the chips by generating a digital Sync signal and sharing this synchronization signal with the slaves. The master also uses a 40 MHz crystal and generates a 40 MHz oscillator clock (OSC_CLKOUT) and shares it with the slaves (as CLKP), thereby eliminating the need for additional crystals on the slaves and ensuring that the entire system operates from a single clock source.

The master is capable of supplying the shared LO on two different output pins through two different delay matched amplifiers. This can be used in a four chip cascade system to supply the LO signal to the master and three slaves using only passive splitters. This eliminates the need for additional, costly, active components on the PCB. The OSC_CLKOUT pin is used by the master to share the the 40 MHz clock source with the slave devices in the system. In the case of a 2-device system, this can be done with just a passive trace between devices. In the case of more than 2-devices, it is recommended to use a clock fan-out buffer to manage loading and signal integrity issues. Similarly, the DIG_SYNC is conveyed from the master to the slaves and back to itself through delay matched buffers on board.

Other than these connections which are illustrated in the below diagrams and further elaborated in later sections, the cascaded system also has Power Management ICs (PMIC) (each PMIC can handle up to two AWR2243 chips), an optional QSPI Flash (needed for initial software development purpose only) and the mmWave antennas connected to each AWR2243 chip.

figure1.gifFigure 1. A Two Chip Cascade System
awr2243-cascade-system.gifFigure 2. A Four Chip Cascade System

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale