Follow these steps to create a product
listing using a Component QDID:
- Navigate to the Bluetooth SIG
qualification page [9] - Select "Path 2: Qualification Process with Required
Testing".
- Open Launch Studio [13].
- Give your project a name and enter
the appropriate BLE-Stack QDID from the list shown in Section 2.1.2. In addition, if a RF-PHY component QDID corresponding to your design is
provided in Section 2.1.2, reference it as well.
- Tick off the appropriate Test
Case Reference List (TCRL) version, typically the latest, and select the product
type and configuration (typically: end product, LE Controller, LE Host). Once
the TCRL Version, Product Types, Controller Core Configuration and Host Core
Configuration are selected additional input fields appear – these are above the
TCRL Version selection. These fields correspond to the layers supported by the
QDIDs selected. By default, the option “Use my own selection” is active.
Choosing the alternate option allows to reuse the ICS Selection made by TI. The
ICS Selection should be reviewed and modified based on the design to qualify.
End product designers are responsible for complying with the Bluetooth SIG
requirements. Once all the selection done, press "Save and Continue (...)".
- In the layer selection page, Core
Specifications can typically be left as is. If you are using any adopted
profiles or services you need to tick off the respective fields. Press "Save and
Continue (...)".
- In the ICS Selection page, keep the
“Consistency Check” tool open. This tool indicates which capabilities checkboxes
are inconsistent with other capabilities checked, or missing mandatory
capabilities. Click on the “Refresh consistency report” button to update the
messages displayed by the tool. Should there be any other inconsistency issues,
see the TI E2E Bluetooth forum [24] for additional information. When done, click "Save and Continue (...)".
- In the Testing page, you can
download the test plan that lists the required tests you need to perform on your
product (typically limited to RF PHY testing). When you have downloaded the test
plan, click "Save and Continue (...)".
- Upload the filled out test plan and
click "Save and Continue (...)".
- The next steps are all about your
specific product. Fill in the required information in the last remaining pages
and you will end up with your very own Declaration ID in the end.
Congratulations!