SWRA615A June 2019 CC1352P , CC1352R , CC2530 , CC2531 , CC2538 , CC2652P , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP
Several reset options are made possible through BDB to perform various reset actions. This includes Basic Cluster resets through the "reset to factor defaults" instruction, in which all cluster attributes on the device are reset to their default values. Network settings, groups, and bindings are not affected. There is also "reset to factory new", where all persistent data is cleared with the exception of the outgoing NWK frame counter. It can be initiated by the Network Leave command with rejoin off, the Mgmt_Leave_req command with rejoin off, local action, or touchlink interface. Finally, there is the "complete" reset. That includes outgoing NWK frame counters and is defined by the manufacturer, as there is no standard method.