SWRA648 May 2019 CC1352P , CC1352R , CC1354P10 , CC1354R10 , CC2642R , CC2642R-Q1 , CC2652P , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP
The overall connection diagram is shown in Figure 12. In this setup, there are four father nodes and each father node is connected to seven child nodes. The key parameters used in this example are shown below:
The tree structure network write and notify function on CC2652R1F test result is shown in Figure 13. From the information shown in the serial port, the grandpa node writes to each father node and each father node in turn forwards the data to its child nodes. Meanwhile, each child node notifies the data to its father node and the father node in turn forwards each notification to the grandpa node.