SWRA659A March 2020 – June 2020 CC3100 , CC3100MOD , CC3200 , CC3200MOD
The following section describes the CC3X00 active and low power static modes. The CC3X00 devices contain only the Networking sub-system and is self-contained in terms of power optimization. The following system modes are defined, and could be measured using TI's EVM boards. The main three building blocks of most power related application profiles are:
More details can be found at: SimpleLink™ CC3100/CC3200 Wi-Fi Internet-on-a-chip™ Networking Sub-system Power Management