SWRA662A January   2020  – September 2022 AWR1243 , AWR1443 , AWR1642 , AWR1843 , AWR1843AOP , AWR2243 , AWR6843 , AWR6843AOP , IWR1443 , IWR1642 , IWR1843 , IWR6443 , IWR6843 , IWR6843AOP

 

  1.   Interference Mitigation For AWR/IWR Devices
  2.   Trademarks
  3. 1Introduction
  4. 2Types of Interference in FMCW Radar
    1. 2.1 FMCW Radar
    2. 2.2 The Radar Equation for Interference
    3. 2.3 Types of Interference
      1. 2.3.1 Crossing Interference
      2. 2.3.2 Performance Analysis for Crossing Interference
      3. 2.3.3 Parallel Interference
      4. 2.3.4 Between Crossing and Parallel Interference
  5. 3Interference Avoidance
    1. 3.1 Standardization: Different Frequency Band and Time Slot for Different Radars
    2. 3.2 Different Starting Time for Parallel Interference
    3. 3.3 Sensing and Avoidance
    4. 3.4 Antenna Polarization
  6. 4Localization and Interference Mitigation
    1. 4.1 Localization
    2. 4.2 Mitigation
  7. 5Dithering and Randomization
  8. 6Conclusion
  9. 7References
  10. 8Revision History

Sensing and Avoidance

In the absence of any synchronization, users can still perform ‘sense and avoid’. In this scheme, before a device begins transmission, it senses the spectrum. This is achieved by keeping the receivers active and the transmitter switched off.

If there have been no transmissions by other radars, the spectrum is silent. The ADC data should only show the thermal noise floor and the noise figure. If, on the other hand, there are transmissions from another radar device, expect spikes in the ADC data corresponding to the points where the crossing occurs.

XWR devices can generate fast chirps of the order of 250 megahertz per microsecond, allowing for fast scans.

A max hold of ADC data cross chirps shows the interferer clearly. In Figure 3-3, the interferer is chirping between frequencies f1 and f2. Thus, the ADC output shows the energies between f1 and f2. If the period of scanning is long enough to cover multiple frames, estimate the number of aggressor radars using the number of discrete bands of frequencies used. The user can also estimate frame periodicity bandwidth occupied by chirps. Most importantly, the user can find free spectra, or time slots, where interference-free transmission is possible.

GUID-8C096252-7435-4E4C-86CE-B3B3701517D6-low.pngFigure 3-3 Sense and Avoid

When the interferers have been identified, the radar can start transmission in regions where the interferer is not active.