SWRA662A January 2020 – September 2022 AWR1243 , AWR1443 , AWR1642 , AWR1843 , AWR1843AOP , AWR2243 , AWR6843 , AWR6843AOP , IWR1443 , IWR1642 , IWR1843 , IWR6443 , IWR6843 , IWR6843AOP
First, let us define two terms: a victim and an aggressor. A victim is a radar device whose receiver is affected by interferers. An aggressor is a radar device whose transmit affects the victim's receiver.
The received signal strength in dBm (PInterference) of an interfering radar can be computed using Equation 1.
where
The distance between the aggressor and the victim is R, and the average RF wavelength is λ.
The radar equation for targets is shown in Equation 2.
Comparing the two equations shows that the path loss effect (that is, the effect of R) is weaker for interferers than targets. In other words, interference is likely to dominate the received signal even if it is far away.