SWRA679 January 2021 CC3200 , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235S , CC3235SF
Based on the chosen capacitor value and the approximate value of Vcc, the expected Vdrop across N samples can be calculated by using Equation 1. Then, the Vcc can be estimated as shown in Equation 2.
The method can be recursively used to improve the value of Vcc, if there is no prior information on Vcc.