SWRA680 November 2020 CC3100 , CC3120 , CC3135 , CC3200 , CC3220R , CC3220S , CC3220SF , CC3235S , CC3235SF
Based on the PCB trace capacitance and the crystal used on the final product, the shunt caps on the crystal may need to be adjusted in order to make sure the net capacitance load is exactly what is required.
The devices require two separate clocks for its operation: