SWRA680 November 2020 CC3100 , CC3120 , CC3135 , CC3200 , CC3220R , CC3220S , CC3220SF , CC3235S , CC3235SF
In order for Radio Tool to operate correctly, the devices need to be flashed with the correct firmware. For instructions on how to flash firmware onto the device, see the SimpleLink Wi-Fi CC31xx, CC32xx UniFlash User’s Guide [14].
For the CC3x20 and CC3x35 devices, make sure to download and install SimpleLink Wi-Fi radio testing tool for CC31xx and CC32xx. For instructions on the installation process, see the CC3x20, CC3x35 SimpleLink Wi-Fi and Internet-on-a chip Solution Radio Tool [15].