SWRA680 November 2020 CC3100 , CC3120 , CC3135 , CC3200 , CC3220R , CC3220S , CC3220SF , CC3235S , CC3235SF
The recommended oscillation mode of operation for the crystal is the fundamental mode. This simplifies the resonant circuit that is required for the crystal. In addition, fundamental crystals typically have lower equivalent series resistance (ESR) than third overtone crystals.