SWRA689 February 2022 AWR6843 , AWR6843AOP , IWR6843 , IWR6843AOP
Acquisition period can be simplified to Equation 1.
Where,
TA : Represents the total acquisition period
Tc : Represents the duration of a single chirp
Nc : Represents the total number of chirps per Tx
NTx : Represents the number of Tx antenna
Reducing any of these parameters will result in a reduction of power consumption seen during the acquisition period, while reducing more than one parameter will have a multiplicative effect overall. Moreover reduction of power in active mode is the most effective way to reduce average power consumption.