SWRA730 February 2022 CC1311P3 , CC1311R3 , CC1312R , CC1312R7 , CC1314R10 , CC1352P , CC1352P7 , CC1352R , CC1354P10 , CC1354R10
The antenna in this application note can be used in two different modes: single-band operation or dual-band operation. When configured as single-band mode, users can configure the antenna through thematching network and Z64 to operate at a single ISM frequency between 433 MHz and 930 MHz. Users can configure the antenna in dual-band mode then the ISM frequency operation can be between 433–930 MHz and also 2.4 GHz. All modes of operation have shown a high transmitted radiated efficiency while maintaining a wide bandwidth.
The antenna design including the antenna matching network can easily be adapted to a specific ISM frequency with the option of single-band or dual-band operation. This is an advantage for designs that require just one PCB antenna structure to cover several bands by just changing the BOM. Even frequencies lower than 433 MHz can be supported, if the Z64 component is increased furthermore.
The dual-band mode is ideal when the radio solution works at sub-1 GHz ISM frequency and 2.4 GHz. When using the dual-band mode it is important that the 3rd harmonic of the 868 MHz (2.604 GHz) antenna is below the regulatory limits since the 2.4 GHz antenna (2.74 GHz to 2.38 GHz) will also radiate the 3rd harmonic.
TI recommends following the antenna dimensions as shown in Figure 1-1; Size of the antenna is 43 x 25 mm. The maximum gain is approximately 3 to 5 dBi, which is typical for a monopole antenna.
S11 measurements show that the center frequency is dependent on the size of the ground plane, but this is easily compensated for by adjusting the antenna length or the antenna match network.