SWRA730 February 2022 CC1311P3 , CC1311R3 , CC1312R , CC1312R7 , CC1314R10 , CC1352P , CC1352P7 , CC1352R , CC1354P10 , CC1354R10
The CTIA measurement summary results are presented in this section. Note that the performance will be affected by the size and shape of the ground plane.
When matching the antenna to 50 ohm a Smith chart tool will give a good indication on the component values needed to match the antenna. However, there will be a deviation between the theoretical impedance given by the Smith chart and realized value. Therefore, further tuning might be necessary in order to archive a good match.