SWRA732 December 2021 CC1352P , CC1352R , CC1354P10 , CC1354R10 , CC2642R , CC2652R , CC2652R7 , CC2652RSIP
For the latest supported CCS version, see the latest SDK’s Release Notes that can be found on the CC13XX-CC26XX-SDK tool page
For the latest supported IAR version, see the latest SDK’s Release Notes that can be found on the CC13XX-CC26XX-SDK tool page
The SysConfig Utility is a software tool which provides a Graphical User Interface for configuring pins, peripherals, radios, subsystems, and other components for TI devices. Results output as C header and code files that can be imported into software development kits (SDKs) or used to configure custom software.
With regards to Bluetooth Mesh, refer to the SDK’s User’s Guide for an overview of the configurable parameters that may be modified using SysConfig. [13]
Paired with a simple_mesh_node example configured with ERPC support, this Python script runs on v3.7.6 [10], allowing you to control your mesh node in a network processor configuration by sending commands to the node through a serial interface