SWRA737A February 2022 – August 2022 CC1352P , CC1352R , CC2640R2F , CC2640R2L , CC2642R , CC2652P , CC2652R , CC2652R7 , CC2652RSIP
[2] introduces the details about BTool. [4] introduce how to use BTool for Bluetooth LE basic operation, which includes where to find the host_test example and how to flash it.
After CC26xx/CC13xx device is flashed with host_test FW, it can receive HCI commands through the UART interface. To verify if the environment is ready, send a basic command, like HCI_readBdAddr. If everything is fine, CC26xx/CC13xx replies its BD Address. Since the BD Address is unique, this command is also useful when you want to record the production history for each device on manufacturing line.