SWRA769 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Application
  5. 2Running the Bluetooth Code
  6. 3Server Set-Up Using HFP Demo Application
  7. 4Client Set-Up on the Demo Application
  8. 5Example: Audio Gateway with a Commercial Headset
  9. 6Application Commands
    1. 6.1  Generic Access Profile Commands
    2. 6.2  Help (DisplayHelp)
    3. 6.3  Inquiry
    4. 6.4  Pair
    5. 6.5  End Pairing
    6. 6.6  PIN Code Response
    7. 6.7  Pass Key Response
    8. 6.8  User Confirmation Response
    9. 6.9  Set Discoverability Mode
    10. 6.10 Set Connectability Mode
    11. 6.11 Set Pairability Mode
    12. 6.12 Change Simple Pairing Parameters
    13. 6.13 Get Local Address
    14. 6.14 Set Local Name
    15. 6.15 Get Local Name
    16. 6.16 Set Class of Device
    17. 6.17 Get Class of Device
    18. 6.18 Get Remote Name
  10. 7Hands-Free Profile Commands
    1. 7.1  Service Discovery
    2. 7.2  Open Audio Gateway Client
    3. 7.3  Manage Audio
    4. 7.4  Update Control Indicators
    5. 7.5  Call Waiting
    6. 7.6  Set Voice Recognition Activation
    7. 7.7  Set Speaker Gain
    8. 7.8  Set Microphone Gain
    9. 7.9  Disable Remote Sound Enhancement
    10. 7.10 Send Caller ID Notification
    11. 7.11 Set Ring Indication
    12. 7.12 Ring Indication
    13. 7.13 Send Incoming Call State
    14. 7.14 Close AG Client
    15. 7.15 Send Operator Info
    16. 7.16 Send Sub Number
    17. 7.17 Send Call List
  11. 8References
  12. 9Revision History

Set Ring Indication

Description

The following function is responsible for sending an enable or disable In-Band Ring Indication to the Remote Hands-Free unit. This function returns zero on successful execution and a negative value on all errors.

Parameters

The command requires only one parameter. This value must be specified as 0 (for disable) or 1 (for enabling).

Command Call Examples

  • "SetRingIndication 1" for enabling In-Band Ring Indication
  • "SetRingIndication 0" for disable In-Band Ring Indication

Possible Return Values

  • (0) Command sent successfully
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-4) FUNCTION_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-1000) BTHFRE_ERROR_INVALID_PARAMETER
  • (-1001) BTHFRE_ERROR_NOT_INITIALIZED
  • (-1002) BTHFRE_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1003) BTHFRE_ERROR_LIBRARY_INITIALIZATION_ERROR
  • (-1004) BTHFRE_ERROR_INSUFFICIENT_RESOURCES
  • (-1005) BTHFRE_ERROR_INVALID_OPERATION
  • (-1006) BTHFRE_ERROR_INVALID_CODEC_ID

API Call

HFRE_Enable_Remote_InBand_Ring_Tone_Setting(BluetoothStackID, CurrentClientPortID, TempParam->Params[0].intParam? TRUE : FALSE)

API Prototype

BTPSAPI_DECLARATION int BTPSAPI HFRE_Enable_Remote_InBand_Ring_Tone_Setting(unsigned int BluetoothStackID, unsigned int HFREPortID, Boolean_tEnableInBandRing)

Description of API

This function is responsible for Enabling or Disabling In-Band Ring Tone Capabilities for the Local Device. This function can only be performed by Audio Gateways for which a validService Level Connection exists. This function can only be used to enable In-Ring Tone Capabilities if the Local Audio Gateway supports this feature. This function accepts as input parameters the Bluetooth Stack ID for which the HFRE Port ID is valid as well as the HFRE Port ID. The final parameter is a Boolean flag specifying if this is a call to Enable or Disable this functionality. This function returns zero if successful or a negative return error code if there was an error.