SWRA769 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Application
  5. 2Running the Bluetooth Code
  6. 3Server Set-Up Using HFP Demo Application
  7. 4Client Set-Up on the Demo Application
  8. 5Example: Audio Gateway with a Commercial Headset
  9. 6Application Commands
    1. 6.1  Generic Access Profile Commands
    2. 6.2  Help (DisplayHelp)
    3. 6.3  Inquiry
    4. 6.4  Pair
    5. 6.5  End Pairing
    6. 6.6  PIN Code Response
    7. 6.7  Pass Key Response
    8. 6.8  User Confirmation Response
    9. 6.9  Set Discoverability Mode
    10. 6.10 Set Connectability Mode
    11. 6.11 Set Pairability Mode
    12. 6.12 Change Simple Pairing Parameters
    13. 6.13 Get Local Address
    14. 6.14 Set Local Name
    15. 6.15 Get Local Name
    16. 6.16 Set Class of Device
    17. 6.17 Get Class of Device
    18. 6.18 Get Remote Name
  10. 7Hands-Free Profile Commands
    1. 7.1  Service Discovery
    2. 7.2  Open Audio Gateway Client
    3. 7.3  Manage Audio
    4. 7.4  Update Control Indicators
    5. 7.5  Call Waiting
    6. 7.6  Set Voice Recognition Activation
    7. 7.7  Set Speaker Gain
    8. 7.8  Set Microphone Gain
    9. 7.9  Disable Remote Sound Enhancement
    10. 7.10 Send Caller ID Notification
    11. 7.11 Set Ring Indication
    12. 7.12 Ring Indication
    13. 7.13 Send Incoming Call State
    14. 7.14 Close AG Client
    15. 7.15 Send Operator Info
    16. 7.16 Send Sub Number
    17. 7.17 Send Call List
  11. 8References
  12. 9Revision History

Send Incoming Call State

Description

The following function is responsible for sending the Response and Hold Command (+BTRH) to the remote device. This function returns zero on successful execution and a negative value on all errors.

Parameters

This command requires only one parameter to which is an integer value that represents the incoming call state. This value must be specified as 0 (incoming call is put on hold), 1 (held call is accept) and 2 (held call is reject).

Command Call Examples

"SendIncomingCallState 1" if there is a incoming call.

Possible Return Values

  • (0) Command sent successfully
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-4) FUNCTION_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-1000) BTHFRE_ERROR_INVALID_PARAMETER
  • (-1001) BTHFRE_ERROR_NOT_INITIALIZED
  • (-1002) BTHFRE_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1003) BTHFRE_ERROR_LIBRARY_INITIALIZATION_ERROR
  • (-1004) BTHFRE_ERROR_INSUFFICIENT_RESOURCES
  • (-1005) BTHFRE_ERROR_INVALID_OPERATION
  • (-1006) BTHFRE_ERROR_INVALID_CODEC_ID

API Call

HFRE_Send_Incoming_Call_State(BluetoothStackID, CurrentClientPortID, (HFRE_Call_State_t) CallState)

API Prototype

BTPSAPI_DECLARATION int BTPSAPI HFRE_Send_Incoming_Call_State(unsigned int BluetoothStackID, unsigned int HFREPortID, HFRE_Call_State_t CallState)

Description of API

The following function is responsible for sending information about the incoming call state. This function can only be performed by Audio Gateways that have a valid Service LevelConnection. This function accepts the Bluetooth Stack ID input parameter for which the HFRE Port ID is valid as well as the HFRE Port ID. The final parameter to this function indicates the call state to set as part of this message. This function returns zero if successful or a negative return error code if there was an error.