SWRA769 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Application
  5. 2Running the Bluetooth Code
  6. 3Server Set-Up Using HFP Demo Application
  7. 4Client Set-Up on the Demo Application
  8. 5Example: Audio Gateway with a Commercial Headset
  9. 6Application Commands
    1. 6.1  Generic Access Profile Commands
    2. 6.2  Help (DisplayHelp)
    3. 6.3  Inquiry
    4. 6.4  Pair
    5. 6.5  End Pairing
    6. 6.6  PIN Code Response
    7. 6.7  Pass Key Response
    8. 6.8  User Confirmation Response
    9. 6.9  Set Discoverability Mode
    10. 6.10 Set Connectability Mode
    11. 6.11 Set Pairability Mode
    12. 6.12 Change Simple Pairing Parameters
    13. 6.13 Get Local Address
    14. 6.14 Set Local Name
    15. 6.15 Get Local Name
    16. 6.16 Set Class of Device
    17. 6.17 Get Class of Device
    18. 6.18 Get Remote Name
  10. 7Hands-Free Profile Commands
    1. 7.1  Service Discovery
    2. 7.2  Open Audio Gateway Client
    3. 7.3  Manage Audio
    4. 7.4  Update Control Indicators
    5. 7.5  Call Waiting
    6. 7.6  Set Voice Recognition Activation
    7. 7.7  Set Speaker Gain
    8. 7.8  Set Microphone Gain
    9. 7.9  Disable Remote Sound Enhancement
    10. 7.10 Send Caller ID Notification
    11. 7.11 Set Ring Indication
    12. 7.12 Ring Indication
    13. 7.13 Send Incoming Call State
    14. 7.14 Close AG Client
    15. 7.15 Send Operator Info
    16. 7.16 Send Sub Number
    17. 7.17 Send Call List
  11. 8References
  12. 9Revision History

Update Control Indicators

Description

The following function is responsible for updating the current state of the Control Indicators on the Remote Hands-Free unit. This function returns zero on successful execution and anegative value on all errors. indicators name : Call status, Call set-up, Service availability, Signal indicator, Roam indicator, Batch indicator and Call Held.

Parameters

The command requires two parameters: indicator name and value.

Command Call Examples

  • "UpdateControlIndicators Call set-up 1"
  • "UpdateControlIndicators Call Held 3"

Possible Return Values

  • (0) Command sent successfully
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-4) FUNCTION_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-1000) BTHFRE_ERROR_INVALID_PARAMETER
  • (-1001) BTHFRE_ERROR_NOT_INITIALIZED
  • (-1002) BTHFRE_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1003) BTHFRE_ERROR_LIBRARY_INITIALIZATION_ERROR
  • (-1004) BTHFRE_ERROR_INSUFFICIENT_RESOURCES
  • (-1005) BTHFRE_ERROR_INVALID_OPERATION
  • (-1006) BTHFRE_ERROR_INVALID_CODEC_ID

API Call

HFRE_Update_Current_Control_Indicator_Status(BluetoothStackID, PortToUse, 1, &HFREIndicatorUpdate)

API Prototype

BTPSAPI_DECLARATION int BTPSAPI HFRE_Update_Current_Control_Indicator_Status(unsigned int BluetoothStackID, unsigned int HFREPortID, unsigned intNumberUpdateIndicators, HFRE_Indicator_Update_t UpdateIndicators[])

Description of API

The following function is responsible for Updating the Current Control Indicator Status. This function may only be performed by Audio Gateways that have a valid Service LevelConnection or by Audio Gateways that have received the etHFRE_Control_Indicator_Request_Indication event. This function accepts as its input parameters the Bluetooth Stack ID forwhich the HFRE Port ID is valid as well as the HFRE Port ID. The third parameter to this function is the number of name/value pairs that are present in the list. The final parameter to this function is a list of name/value pairs for the indicators to be updated. This function returns zero if successful or a negative return error code if there was an error.