SWRA769 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Application
  5. 2Running the Bluetooth Code
  6. 3Server Set-Up Using HFP Demo Application
  7. 4Client Set-Up on the Demo Application
  8. 5Example: Audio Gateway with a Commercial Headset
  9. 6Application Commands
    1. 6.1  Generic Access Profile Commands
    2. 6.2  Help (DisplayHelp)
    3. 6.3  Inquiry
    4. 6.4  Pair
    5. 6.5  End Pairing
    6. 6.6  PIN Code Response
    7. 6.7  Pass Key Response
    8. 6.8  User Confirmation Response
    9. 6.9  Set Discoverability Mode
    10. 6.10 Set Connectability Mode
    11. 6.11 Set Pairability Mode
    12. 6.12 Change Simple Pairing Parameters
    13. 6.13 Get Local Address
    14. 6.14 Set Local Name
    15. 6.15 Get Local Name
    16. 6.16 Set Class of Device
    17. 6.17 Get Class of Device
    18. 6.18 Get Remote Name
  10. 7Hands-Free Profile Commands
    1. 7.1  Service Discovery
    2. 7.2  Open Audio Gateway Client
    3. 7.3  Manage Audio
    4. 7.4  Update Control Indicators
    5. 7.5  Call Waiting
    6. 7.6  Set Voice Recognition Activation
    7. 7.7  Set Speaker Gain
    8. 7.8  Set Microphone Gain
    9. 7.9  Disable Remote Sound Enhancement
    10. 7.10 Send Caller ID Notification
    11. 7.11 Set Ring Indication
    12. 7.12 Ring Indication
    13. 7.13 Send Incoming Call State
    14. 7.14 Close AG Client
    15. 7.15 Send Operator Info
    16. 7.16 Send Sub Number
    17. 7.17 Send Call List
  11. 8References
  12. 9Revision History

Manage Audio

Description

The following function is responsible for setting up or releasing an audio connection. This function returns zero on successful execution and a negative value on all errors.

Parameters

The Manage Audio command requires only one parameter to which is an integer value that represents the ManageAudio mode. This value must be specified as 0 (for Release) or 1 (for set-up).

Command Call Examples

  • "ManageAudio 0" Attempts to Release the Audio Connection.
  • "ManageAudio 1" Attempts to set-up the Audio Connection.

Possible Return Values

  • (0) Command sent successfully
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-4) FUNCTION_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-1000) BTHFRE_ERROR_INVALID_PARAMETER
  • (-1001) BTHFRE_ERROR_NOT_INITIALIZED
  • (-1002) BTHFRE_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1003) BTHFRE_ERROR_LIBRARY_INITIALIZATION_ERROR
  • (-1004) BTHFRE_ERROR_INSUFFICIENT_RESOURCES
  • (-1005) BTHFRE_ERROR_INVALID_OPERATION
  • (-1006) BTHFRE_ERROR_INVALID_CODEC_ID

API Call

HFRE_set-up_Audio_Connection(BluetoothStackID, CurrentClientPortID) or HFRE_Release_Audio_Connection(BluetoothStackID, CurrentClientPortID)

API Prototype

int BTPSAPI HFRE_set-up_Audio_Connection(unsigned int BluetoothStackID, unsigned int HFREPortID) or int BTPSAPI HFRE_Release_Audio_Connection(unsigned int BluetoothStackID, unsigned int HFREPortID)

Description of API

This function is responsible for Setting Up an Audio Connection between the Local and Remote Device. This function can be used by either an Audio Gateway or a Hands-Free unit for which a valid Service Level Connection Exists. This function accepts as its input parameters the Bluetooth Stack ID for which the HFRE Port ID is valid as well as the HFRE Port ID. This function returns zero if successful or a negative return error code if there was an error.

(or) This function is responsible for Releasing an Audio Connection which was previously established by the Remote Device or by a call to the HFRE_set-up_Audio_Connection()function. This function can be used by either an Audio Gateway or a Hands-Free unit. This function accepts as its input parameters the Bluetooth Stack ID for which the HFRE Port ID is valid as well as the HFRE Port ID. This function returns zero if successful or a negative return error code if there was an error.