SWRA769 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Application
  5. 2Running the Bluetooth Code
  6. 3Server Set-Up Using HFP Demo Application
  7. 4Client Set-Up on the Demo Application
  8. 5Example: Audio Gateway with a Commercial Headset
  9. 6Application Commands
    1. 6.1  Generic Access Profile Commands
    2. 6.2  Help (DisplayHelp)
    3. 6.3  Inquiry
    4. 6.4  Pair
    5. 6.5  End Pairing
    6. 6.6  PIN Code Response
    7. 6.7  Pass Key Response
    8. 6.8  User Confirmation Response
    9. 6.9  Set Discoverability Mode
    10. 6.10 Set Connectability Mode
    11. 6.11 Set Pairability Mode
    12. 6.12 Change Simple Pairing Parameters
    13. 6.13 Get Local Address
    14. 6.14 Set Local Name
    15. 6.15 Get Local Name
    16. 6.16 Set Class of Device
    17. 6.17 Get Class of Device
    18. 6.18 Get Remote Name
  10. 7Hands-Free Profile Commands
    1. 7.1  Service Discovery
    2. 7.2  Open Audio Gateway Client
    3. 7.3  Manage Audio
    4. 7.4  Update Control Indicators
    5. 7.5  Call Waiting
    6. 7.6  Set Voice Recognition Activation
    7. 7.7  Set Speaker Gain
    8. 7.8  Set Microphone Gain
    9. 7.9  Disable Remote Sound Enhancement
    10. 7.10 Send Caller ID Notification
    11. 7.11 Set Ring Indication
    12. 7.12 Ring Indication
    13. 7.13 Send Incoming Call State
    14. 7.14 Close AG Client
    15. 7.15 Send Operator Info
    16. 7.16 Send Sub Number
    17. 7.17 Send Call List
  11. 8References
  12. 9Revision History

Send Sub Number

Note: This function is performed when a request is received to query the subscriber number information from the remote Hands-free device.

Description

The following function is responsible for sending the command to send a subscriber number to the Remote Hands-free Device. when received a request to query the subscriber number information from the remote Hands-free device. This function returns zero on successful execution and a negative value on all errors.

Parameters

The Send Subscriber Number command requires only one parameter which is the phone number to be sent as part of this response.

Command Call Examples

"SendSubNumber +9198787899889"

Possible Return Values

  • (0) Command sent successfully
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-4) FUNCTION_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-1000) BTHFRE_ERROR_INVALID_PARAMETER
  • (-1001) BTHFRE_ERROR_NOT_INITIALIZED
  • (-1002) BTHFRE_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1003) BTHFRE_ERROR_LIBRARY_INITIALIZATION_ERROR
  • (-1004) BTHFRE_ERROR_INSUFFICIENT_RESOURCES
  • (-1005) BTHFRE_ERROR_INVALID_OPERATION
  • (-1006) BTHFRE_ERROR_INVALID_CODEC_ID

API Call

HFRE_Send_Subscriber_Number_Information(BluetoothStackID, CurrentClientPortID, TempParam->Params[0].strParam, 4, HFRE_DEFAULT_NUMBER_FORMAT, TRUE)

API Prototype

BTPSAPI_DECLARATION int BTPSAPI HFRE_Send_Subscriber_Number_Information(unsigned int BluetoothStackID, unsigned int HFREPortID, char *PhoneNumber, unsigned intServiceType, unsigned int NumberFormat, Boolean_t FinalEntry)

Description of API

The following function is responsible for sending Subscriber Number Information. This function can only be performed by Audio Gateways that have received a request to query the subscriber number information. This function accepts the Bluetooth Stack ID parameters for which the HFRE Port ID is valid as well as the HFRE Port ID. The third parameter to this function is the phone number to be sent as part of this response. The Phone Number Parameter String Length *MUST* be between the values ofHFRE_PHONE_NUMBER_LENGTH_MINIMUM and HFRE_PHONE_NUMBER_LENGTH_MAXIMUM. The fourth parameter to this function is the Service type related to the specified Phone Number. The fifth parameter to this function is the Number Format to use for this number, the final parameter to this function is a boolean indicating if this is the last subscriber number information entry to be sent therefore requiring that an OK be sent as well. This function returns zero if successful or a negative return error code if there was an error.