SWRA770 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Overview
  5. 2Running the Bluetooth Code
  6. 3Demo Application
    1. 3.1 Device 1 (Host/HID Host) Setup on the Demo Application
    2. 3.2 Device 2 (Client/HID Device Setup on the Demo Application
    3. 3.3 Initiating Connection from the HID Host
    4. 3.4 Initiating Connection from HID Device
    5. 3.5 Communication Between Host and Device
  7. 4Application Commands
  8. 5Gap Commands
    1. 5.1  Help (DisplayHelp)
    2. 5.2  Inquiry
    3. 5.3  Display Inquiry List
    4. 5.4  Pair
    5. 5.5  End Pairing
    6. 5.6  PIN Code Response
    7. 5.7  Pass Key Response
    8. 5.8  User Confirmation Response
    9. 5.9  Set Discoverability Mode
    10. 5.10 Set Connectability Mode
    11. 5.11 Set Pairability Mode
    12. 5.12 Change Simple Pairing Parameters
    13. 5.13 Get Local Address
    14. 5.14 Set Local Name
    15. 5.15 Get Local Name
    16. 5.16 Set Class of Device
    17. 5.17 Get Class of Device
    18. 5.18 Get Remote Name
  9. 6Human Interface Demo Profile
    1. 6.1 Host
      1. 6.1.1  Connect Remote HID Device
      2. 6.1.2  Close Connection
      3. 6.1.3  Control Request
      4. 6.1.4  Get Report Request
      5. 6.1.5  Set Report Request
      6. 6.1.6  Get Protocol Request
      7. 6.1.7  Set Protocol Request
      8. 6.1.8  Get Idle Request
      9. 6.1.9  Set Idle Request
      10. 6.1.10 Data Write
    2. 6.2 Client
      1. 6.2.1 Get Report Response
      2. 6.2.2 Set Report Response
      3. 6.2.3 Get Protocol Response
      4. 6.2.4 Set Protocol Response
      5. 6.2.5 Get Idle Response
      6. 6.2.6 Set Idle Response
  10. 7References
  11. 8Revision History

Set Local Name

Description

The SetLocalName command is responsible for setting the name of the local Bluetooth Device to a specified name. This function returns zero on a successful execution and a negative value on all errors. A Bluetooth Stack ID must exist before attempting to call this function.

Parameters

One parameter is necessary for this command. The specified device name must be the only parameter.

Note: Do not add spaces to the name or only the first section of the name is set.

Command Call Examples

  • "SetLocalName New_Bluetooth_Device_Name" Attempts to set the Local Device Name to "New_Bluetooth_Device_Name."
  • "SetLocalName New Bluetooth Device Name" attempts to set the Local Device Name to "New Bluetooth Device Name" but only sets the first parameter, which makes the LocalDevice Name "New."
  • "SetLocalName MSP430" Attempts to set the Local Device Name to "MSP430."

Possible Return Values

  • (0) Successfully Set Local Device Name
  • (-1) BTPS_ERROR_INVALID_PARAMETER
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-8) INVALID_STACK_ID_ERROR
  • (-4) FUNCTION_ERROR
  • (-57) BTPS_ERROR_DEVICE_HCI_ERROR

API Call

GAP_Set_Local_Device_Name(BluetoothStackID, TempParam->Params[0].strParam)

API Prototype

int BTPSAPI GAP_Set_Local_Device_Name(unsigned int BluetoothStackID, char *Name)

Description of API

This function is provided to allow the changing of the device name of the local Bluetooth Device. The name parameter must be a pointer to a NULL terminated ASCII string of at most MAX_NAME_LENGTH (not counting the trailing NULL terminator). This function returns zero if the local device name was successfully changed, or a negative return error code if there was an error condition.