SWRA770 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Overview
  5. 2Running the Bluetooth Code
  6. 3Demo Application
    1. 3.1 Device 1 (Host/HID Host) Setup on the Demo Application
    2. 3.2 Device 2 (Client/HID Device Setup on the Demo Application
    3. 3.3 Initiating Connection from the HID Host
    4. 3.4 Initiating Connection from HID Device
    5. 3.5 Communication Between Host and Device
  7. 4Application Commands
  8. 5Gap Commands
    1. 5.1  Help (DisplayHelp)
    2. 5.2  Inquiry
    3. 5.3  Display Inquiry List
    4. 5.4  Pair
    5. 5.5  End Pairing
    6. 5.6  PIN Code Response
    7. 5.7  Pass Key Response
    8. 5.8  User Confirmation Response
    9. 5.9  Set Discoverability Mode
    10. 5.10 Set Connectability Mode
    11. 5.11 Set Pairability Mode
    12. 5.12 Change Simple Pairing Parameters
    13. 5.13 Get Local Address
    14. 5.14 Set Local Name
    15. 5.15 Get Local Name
    16. 5.16 Set Class of Device
    17. 5.17 Get Class of Device
    18. 5.18 Get Remote Name
  9. 6Human Interface Demo Profile
    1. 6.1 Host
      1. 6.1.1  Connect Remote HID Device
      2. 6.1.2  Close Connection
      3. 6.1.3  Control Request
      4. 6.1.4  Get Report Request
      5. 6.1.5  Set Report Request
      6. 6.1.6  Get Protocol Request
      7. 6.1.7  Set Protocol Request
      8. 6.1.8  Get Idle Request
      9. 6.1.9  Set Idle Request
      10. 6.1.10 Data Write
    2. 6.2 Client
      1. 6.2.1 Get Report Response
      2. 6.2.2 Set Report Response
      3. 6.2.3 Get Protocol Response
      4. 6.2.4 Set Protocol Response
      5. 6.2.5 Get Idle Response
      6. 6.2.6 Set Idle Response
  10. 7References
  11. 8Revision History

Connect Remote HID Device

Description

The following function is responsible for Connecting to a Remote HID Device. This function returns zero on successful execution and a negative value on all errors.

Parameters

This command takes Inquiry Index number to work which can be found using the DisplayInquiryList command after an Inquiry has been completed.

Possible Return Values

  • (0)HID_Connect_Remote_Device: Function Successful
  • (-4) FUNCTION_ERROR
  • (-6)INVALID_PARAMETERS_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-103)BTPS_ERROR_FEATURE_NOT_AVAILABLE
  • (-1000)BTHID_ERROR_INVALID_PARAMETER
  • (-1001)BTHID_ERROR_NOT_INITIALIZED
  • (-1002)BTHID_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1004)BTHID_ERROR_INSUFFICIENT_RESOURCES

API Call

HID_Connect_Remote_Device(BluetoothStackID, InquiryResultList[(TempParam->Params->intParam-1)], &HIDConfiguration, HID_Event_Callback, 0)

API Prototype

int BTPSAPI HID_Connect_Remote_Device(unsigned int BluetoothStackID, BD_ADDR_t BD_ADDR, HID_Configuration_t *HIDConfiguration, HID_Event_Callback_tEventCallback, unsigned long CallbackParameter)

Description of API

The following function is responsible for opening a connection to a Remote HID Device on the Specified Bluetooth Device. This function accepts as the first parameter the Bluetooth StackID of the Bluetooth Stack which opens the HID Connection. The second parameter specifies the Board Address (NON NULL) of the Remote Bluetooth Device to connect with. The third parameter to this function is the HID Configuration Specification to be used in the negotiation of the L2CAP Channels associated with this Device Client. The final two parameters specify the HID Event Callback function and Callback Parameter, respectively, of the HID Event Callback that is to process any further events associated with this Device Client. This function returns a non-zero, positive, value if successful, or a negative return error code if this function is unsuccessful. If this function is successful, the return value represents the HID ID that can be passed to all other functions that require this. Once a Connection is opened to a Remote Device, this can only be closed via a call to the HID_Close_Connection() function (passing in the return value from a successful call to this function as the HID ID input parameter.)