SWRA770 august 2023 CC2564C
Once the code is flashed, connect the board to a PC using a miniUSB or microUSB cable. Once connected, wait for the driver to install. This appears as MSP-EXP430F5438 USB -Serial Port(COM x), Tiva Virtual COM Port (COM x) , XDS110 Class Application/User UART (COM x) for MSP432, under Ports (COM & LPT) in the Device manager. Attach a Terminal program like PuTTY to the serial port x for the board. The serial parameters to use are 115200 Baud (9600 for MSP430), 8, n, 1. Once connected, reset the Device using Reset S3 button (located next to the mini USB connector for the MSP430) and observe the stack initialized on the terminal. The help screen is displayed and shows all of the commands.