SWRA772 august 2023 CC2564C
At this point the client (LightBlue) can send data to the server (SPPLEDemo). To send data from LightBlue to SPPLEDemo do the following:
In the SPPLEDemo terminal, observe a data indication event. To read the data run the LERead 5cfc3252180b command, obeserve the following in the terminal:
Data Indication Event, Connection ID 1, Received 3 bytes.
SPP+LE>LERead 5cfc3252180b
Read: 3.
ABC
Open the Rx Credits Characteristic (0xE06D5EFB-4F4A-45C0-9EB1-371AE5A14AD4) observe that SPPLEDemo has credited LightBlue with 3 more credits: