SWRA772 august 2023 CC2564C
This application demonstrates a BR/EDR SPP based application as well as a custom application, SPPLE, over Bluetooth LE that is similar in functionality to the BR/EDR appliacation.The SPPLE Profile is similar to the SPP profile except the SPPLE uses LE transport compared to BR/EDR transport in the SPP profile. The SPP profile emulates serial cable connections. There are two roles defined in this profile. The first is the server that has the SPPLE service running and has open an server port. The client is a device that connects to the server. Both of these devices can then exchange data with each other.
Visit the TI Dual-Mode Bluetooth® Stack on MSP432™ MCUs or Dual-Mode Bluetooth® Stack on STM32F4 MCUs pages before trying the application described on this page.