SWRA772 august 2023 CC2564C
The SetLocalAppearence command is provided to set the local device appearance that is exposed by the GAP Service (GAPS).
The one parameter the SetLocalAppearence command requires is the Local Device Appearance.
GAPS_Set_Device_Appearance(BluetoothStackID, GAPSInstanceID, Appearance)
int BTPSAPI GAPS_Set_Device_Appearance (unsigned int BluetoothStackID, unsigned int InstanceID, Word_t DeviceAppearance)
This function allows a mechanism of setting the local device appearance that is exposed as part of the GAP Service API (GAPS).