SWRA780A September 2023 – February 2024 CC3300 , CC3301
Secured host interface focuses on the traffic that is transferred from the host MCU/MPU subsystem to the CC33xx companion IC. A potential hacker can hijack the interface HW lines and use those lines to read confidential information like encryption keys, payload of data units and more. A hacker can also write to those lines and cause unwanted behavior of the device or give misleading events to the host controller as is illustrated in Figure 3-3.