SWRA782 October 2023 CC1311P3 , CC1311R3 , CC1312PSIP , CC1312R , CC1312R7 , CC1314R10 , CC1352P , CC1352P7 , CC1352R , CC1354P10
Code Example | Description |
---|---|
Collector (SUB1G/2.4G) | The collector example creates a PAN-Coordinator device using TI 15.4-Stack |
Collector Secure Managed (SUB1G/2.4G) | The example creates a PAN-Coordinator device using TI 15.4-Stack-based star network with secure commissioning |
Sensor (SUB1G/2.4G) | The sensor example can be used to join the PAN network created with the Collector example |
Sensor Secure Managed (SUB1G/2.4G) | The sensor example can be used to join the PAN network created with the Collector Secure managed example |
Coprocessor | Demonstrates how to implement a MAC coprocessor device in a two-chip scenario. In this example, the TI 15.4-Stack runs on a SimpleLink device, which can be interfaced with any device using a serial interface. |
Sensor OAD off-chip secure (2.4G/SUB1) | The Sensor OAD Off-chip example application demonstrates how to implement a sensor network using TI 15.4-Stack with off chip OAD configuration with AM335x and MAC- Coprocessor. |
Sensor OAD on-chip secure (2.4G/SUB1) | The Sensor OAD on-chip example demonstrates how to implement a 15.4 network with on-chip OAD capabilities with AM335x and MAC- Coprocessor. |
Sensor OAD on-chip persistent secure (2.4G/SUB1) | The Sensor on-chip persistence example demonstrates how OAD with AM335x and MAC coprocessor works with an persistent image along the application image. |