SWRA794A June 2024 – September 2024 AWRL1432 , AWRL6432 , IWRL1432 , IWRL6432 , IWRL6432AOP
Factory calibrations are performed to compensate for manufacturing process variation effects. Factory calibrations are recommended to be performed in a controlled environment(an RF interference-free environment) at user's factory. These are typically performed between junction temperatures of 10°C to 50°C (preferably at 25°C). Once the factory calibrations are performed the Rx gain codes and Tx PA codes are derived for three temperature bins (Table 4-2). The user application can store the calibration results in non-volatile memory and restore at cold boot. If the end user system does not have capability to store factory calibration results, then the calibrations need to be run at every cold boot. Figure 6-1 in Section 6.1 talks about various stages and steps for factory calibrations to be performed by user application.