SWRA794A June 2024 – September 2024 AWRL1432 , AWRL6432 , IWRL1432 , IWRL6432 , IWRL6432AOP
The rl_fecssRfRuntimeCal is used to configure and trigger the runtime calibrations. The configuration structure of this API allows you to choose the necessary calibrations which need to be performed based on the temperature bin and change in temperature (see Section 7). The application can read the device temperature using rl_fecssTempMeasTrig API and provide the bin index to the configuration structure of this Runtime Cal API. Run time calibration status is obtained as a response once this API is triggered.
For the duration required to complete each calibrations, refer to the 'Calibration Execution Time' section in the Interface control document.