SWRA796A December 2023 – August 2025 MSPM0C1106 , MSPM0G3507
This subsystem serves as an I2C-to-UART bridge. In this subsystem, the MSPM0 device is the I2C target device. When the I2C controller transmits to the I2C target, the target collects all of the received data. Once the target detects a stop condition, the target transmits the data out using the UART interface. When the I2C controller attempts to read from the bridge, the bridge transmits the last byte received from the UART device. When the I2C controller reads two bytes, the bridge transmits the last byte received from the UART device and the latest error code generated by the bridge.
The MSPM0 is connected to the I2C controller with the I2C SCL and SDA lines. The MSPM0 is also connected to a UART device using the UART TX and RX lines.
Peripheral Used | Notes |
---|---|
I2C | Called I2C_INST in code |
UART | Called UART_INST in code |
Figure 1-2 shows the code flow diagram for this example and explains how the device fills the data buffers with received I2C data, then transfers the data out via UART.
This application makes use of the TI System Configuration Tool (SysConfig) graphical interface to generate the configuration code of the device peripherals. Using a graphical interface to configure the device peripherals streamlines the application prototyping process.
The code for what is described in Figure 1-2 is found in the beginning of main() in the i2c_to_uart_bridge.c file.
This application must allocate memory for the received data and the data to be transmitted out. The application also needs to keep count for how much data was received and transmitted. A flag is necessary to determine when the data being received is completed and ready to transmit out via UART. There is also an enum for error codes, along with a variable to save them. The initialization of the buffers, counters, enum, and flag are shown here:
#include "ti_msp_dl_config.h"
/* Maximum size of TX packet */
#define I2C_TX_MAX_PACKET_SIZE (1)
/* Maximum size of RX packet */
#define I2C_RX_MAX_PACKET_SIZE (16)
/* Data sent to Controller in response to Read transfer */
uint8_t gTxPacket[I2C_TX_MAX_PACKET_SIZE] = {0x00};
/* Counters for TX length and bytes sent */
uint32_t gTxLen, gTxCount;
/* Data received from Controller during a Write transfer */
uint8_t gRxPacket[I2C_RX_MAX_PACKET_SIZE];
/* Counters for TX length and bytes sent */
uint32_t gRxLen, gRxCount;
enum error_codes{
NO_ERROR,
DATA_BUFFER_OVERFLOW,
RX_FIFO_FULL,
NO_DATA_RECEIVED,
I2C_TARGET_TXFIFO_UNDERFLOW,
I2C_TARGET_RXFIFO_OVERFLOW,
I2C_TARGET_ARBITRATION_LOST,
I2C_INTERRUPT_OVERFLOW,
UART_OVERRUN_ERROR,
UART_BREAK_ERROR,
UART_PARITY_ERROR,
UART_FRAMING_ERROR,
UART_RX_TIMEOUT_ERROR
};
uint8_t gErrorStatus = NO_ERROR;
/* Buffer to hold data received from UART device */
uint8_t gUARTRxData = 0;
/* Flags */
bool gUartTxReady = false; /* Flag to start UART transfer */
bool gUartRxDone = false; /* Flag to indicate UART data has been received */
The main body of the application code is relatively short. First the device and the peripherals are initialized. Then interrupts and events are enabled. The counter values are also initialized. Finally, the main loop is reached, where a flag is polled detect when the received data is ready to be transferred back out via UART:
int main(void)
{
SYSCFG_DL_init();
gTxCount = 0;
gTxLen = I2C_TX_MAX_PACKET_SIZE;
DL_I2C_enableInterrupt(I2C_INST, DL_I2C_INTERRUPT_TARGET_TXFIFO_TRIGGER);
/* Initialize variables to receive data inside RX ISR */
gRxCount = 0;
gRxLen = I2C_RX_MAX_PACKET_SIZE;
NVIC_EnableIRQ(I2C_INST_INT_IRQN);
NVIC_EnableIRQ(UART_INST_INT_IRQN);
while (1) {
if(gUartTxReady){
gUartTxReady = false;
for(int i = 0; i < gRxCount; i++){
/* Transmit data out via UART and wait until transfer is complete */
DL_UART_Main_transmitDataBlocking(UART_INST, gTxPacket[i]);
}
}
}
}
The next piece of this code is the I2C IRQ Handler. This code is used to start and then stop data collection. Next, the code saves the data as the data is received. When the pending interrupt is an I2C Start condition detected, the device initializes the counter variables. When the pending interrupt indicates that the RX FIFO has data available, the device checks to see if there is space left in the data buffer. If there is space, the received value is saved. If there is not any more space, the received value is ignored. When the pending interrupt is the TX FIFO Trigger, the device checks to see how many bytes have been sent. If the device has already sent a byte, then the FIFO is filled with the most recently reported error code. When the pending interrupt is an I2C stop condition, the device checks to see if data was received. If data was received, the received data buffer is copied into the transmit data buffer, and the UART TX ready flag is set to true. If no data was received, the device does not send anything. This ISR also handles I2C error interrupts by assigning the appropriate error code to the gErrorStatus variable.
void I2C_INST_IRQHandler(void)
{
static bool dataRx = false;
switch (DL_I2C_getPendingInterrupt(I2C_INST)) {
case DL_I2C_IIDX_TARGET_START:
/* Initialize RX or TX after Start condition is received */
gTxCount = 0;
gRxCount = 0;
dataRx = false;
/* Flush TX FIFO to refill it */
DL_I2C_flushTargetTXFIFO(I2C_INST);
break;
case DL_I2C_IIDX_TARGET_RXFIFO_TRIGGER:
/* Store received data in buffer */
dataRx = true;
while (DL_I2C_isTargetRXFIFOEmpty(I2C_INST) != true) {
if (gRxCount < gRxLen) {
gRxPacket[gRxCount++] = DL_I2C_receiveTargetData(I2C_INST);
} else {
/* Prevent overflow and just ignore data */
DL_I2C_receiveTargetData(I2C_INST);
}
}
break;
case DL_I2C_IIDX_TARGET_TXFIFO_TRIGGER:
/* Fill TX FIFO if there are more bytes to send */
if (gTxCount < gTxLen) {
gTxCount += DL_I2C_fillTargetTXFIFO(
I2C_INST, &gUARTRxData, (gTxLen - gTxCount));
} else {
/*
* Fill FIFO with error status after sending latest received
* byte
*/
while (DL_I2C_transmitTargetDataCheck(I2C_INST, gErrorStatus) != false)
;
}
break;
case DL_I2C_IIDX_TARGET_STOP:
/* If data was received, echo to TX buffer */
if (dataRx == true) {
for (uint16_t i = 0;
(i < gRxCount) && (i < I2C_TX_MAX_PACKET_SIZE); i++) {
gTxPacket[i] = gRxPacket[i];
DL_I2C_flushTargetTXFIFO(I2C_INST);
}
dataRx = false;
}
/* Set flag to indicate data ready for UART TX */
gUartTxReady = true;
break;
case DL_I2C_IIDX_TARGET_RX_DONE:
/* Not used for this example */
case DL_I2C_IIDX_TARGET_RXFIFO_FULL:
/* Not used for this example */
case DL_I2C_IIDX_TARGET_GENERAL_CALL:
/* Not used for this example */
case DL_I2C_IIDX_TARGET_EVENT1_DMA_DONE:
/* Not used for this example */
case DL_I2C_IIDX_TARGET_EVENT2_DMA_DONE:
/* Not used for this example */
case DL_I2C_IIDX_TARGET_TXFIFO_UNDERFLOW:
gErrorStatus = I2C_TARGET_TXFIFO_UNDERFLOW;
break;
case DL_I2C_IIDX_TARGET_RXFIFO_OVERFLOW:
gErrorStatus = I2C_TARGET_RXFIFO_OVERFLOW;
break;
case DL_I2C_IIDX_TARGET_ARBITRATION_LOST:
gErrorStatus = I2C_TARGET_ARBITRATION_LOST;
break;
case DL_I2C_IIDX_INTERRUPT_OVERFLOW:
gErrorStatus = I2C_INTERRUPT_OVERFLOW;
break;
default:
break;
}
}
The final piece of code in this example is the UART IRQ Handler. The UART IRQ handler is only used to save received data, and check for errors. When a UART RX interrupt is pending, the device saves the received data to a buffer, gUARTRxData, then sets a flag to indicate there is new RX data saved. When a UART error does occur, this ISR executes to assign the correct error code to gErrorStatus.
void UART_INST_IRQHandler(void)
{
switch (DL_UART_Main_getPendingInterrupt(UART_INST)) {
case DL_UART_MAIN_IIDX_RX:
DL_UART_Main_receiveDataCheck(UART_INST, &gUARTRxData);
gUartRxDone = true;
break;
case DL_UART_INTERRUPT_OVERRUN_ERROR:
gErrorStatus = UART_OVERRUN_ERROR;
break;
case DL_UART_INTERRUPT_BREAK_ERROR:
gErrorStatus = UART_BREAK_ERROR;
break;
case DL_UART_INTERRUPT_PARITY_ERROR:
gErrorStatus = UART_PARITY_ERROR;
break;
case DL_UART_INTERRUPT_FRAMING_ERROR:
gErrorStatus = UART_FRAMING_ERROR;
break;
case DL_UART_INTERRUPT_RX_TIMEOUT_ERROR:
gErrorStatus = UART_RX_TIMEOUT_ERROR;
break;
default:
break;
}
}
Changes from Revision * (December 2023) to Revision A (August 2025)