SWRA797 September 2024 CC1312PSIP
When the CC1312PSIP is integrated into an end-product, there are two options for the CC1312PSIP certification. The ownership can be transferred to Texas Instruments Inc. or is transferred to the end-user manufacturer. Since Texas Instruments cannot have the certification ownership of the end-user product this has to be transferred to the end-user manufacturer (FCC 2.933).
For an end-user manufacturer to access the certification ownership for the CC1312PSIP, this requires them to obtain a FCC ID for that module which involves the following steps:
If the end-user manufacturer obtained a FCC ID, the FCC ID can apply to the TCB for permissive changes without asking the module manufacturer for a signed approval letter.
Where both a permissive change and a change in FCC ID are required, the change in ID application must be processed first, followed by the permissive change filing.