SWRA797 September 2024 CC1312PSIP
Upon the approval, all the files are available on the https://fccid.io/ZAT-1312PSIP-3 homepage. Please refer to references 4.7 to 4.23 for the documents listed on the FCC homepage. Documents that are shown above marked as Confidential Document are provided to end-customer via the CC1312PSIP Certification homepage [4.6]: https://www.ti.com/tool/CC1312PSIP-CERTIFICATION
This guideline recommends the software and hardware parameters required to re-use the FCC ID on the end-user product. If these guidelines are not followed, the risk of emissions increases and these are discovered when performing the unintentional radiator measurement tests at the test house. Refer to 4.3 for the official and complete CC1312PSIP Manual Information for the End User and OEM Installation Guide.
The CC1312PSIP has a full FCC grant which implies that the certification can be re-used. Then the FCC test reports from the CC1312PSIP can be provided to the FCC test lab. Besides the host labeling and updating of end-product documents, a change in the FCC ID is needed since the ownership of the end-product cannot be transferred to Texas Instruments Inc. and are maintained by the end-product manufacturer (see also FCC 2.933).