SWRA797 September 2024 CC1312PSIP
The CC1312PSIPMOT is designed to operate in the 902MHz to 928MHz band where the FCC modular certification can be re-used. CC1312PSIPMOT can also be used for the 868MHz ISM band but this is not covered by the FCC modular certification. The maximum RF power transmitted is 20dBm but this is dependent on the PHY.
For ETSI operation within 863MHz to 876MHz ISM band. The output power does not exceed 14.0dBm between 863MHz to 870MHz. If greater than 14.0dBm is required, then the operating frequency has to be within 869.400MHz to 869.650MHz. Then 20dBm can be transmitted at 869.525MHz. 20dBm can also be used in the frequency region of 870MHz to 876MHz for certain countries in Europe but not all countries support this frequency region in the EU.