SWRA820A May 2024 – August 2024 IWRL6432AOP
The TX - RX coupling causes a low-frequency signal at the RX output which can be large enough to saturate the receiver ADC if precautions are not taken. The strength of the receiver ADC saturation depends on:
To mitigate this risk, the swing at the receiver output needs to be reduced. This is achieved by the recommendations in the following section.