The noise riding on the coupled signal
can increase the noise figure of the receiver. Increased noise figure reduces the
SNR of the detected object, leading to reduced detection range and accuracy. The
effective isotropic noise figure therefore depends on two things:
- TX Backoff
- TX - RX Isolation
The TX - RX isolation depends on two
factors:
- Transmit and Receive
combination
- RF frequency
Figure 2-1 shows the
dependencies of the effective isotropic noise figure (EINF) across different
transmit and receive combinations and across different RF frequencies. The EINF is
shown for two different TX backoff settings (0dB and 6dB). The change in noise
figure between the two TX backoff settings show the impact of TX-RX coupling on
noise figure for different RF frequencies.
These effects
across transmit and receive pairs can be combined to show a total effect of all
transmit and receive antennas across RF frequency. Figure 2-2 shows the
noise figure averaged across different TX-RX combinations.
Note: Due to the increased noise figure
at 60GHz, TI recommends avoiding narrow bandwidth chirps
(< 0.5GHz) around 60GHz.
Maximizing detection range (or
minimizing required integration time for a particular detection distance) relies on
maximizing detection SNR. Based on the previously-mentioned noise figure profiles,
this can be achieved in several ways.
- Reducing TX power (increasing
power backoff) lowers the noise figure by reducing the amount of coupling
between TX and RX antennas. This varies between TX and RX combination and across
output frequency. However, the benefit by lowered noise figure is outweighed by
the reduction in transmitted power, lowering the detection range.
- Choosing start and stop
frequencies (bandwidth) of the FMCW chirp can help reduce coupling and lower the
noise figure. As Figure 2-2 shows,
the 61 to 64GHz band has lower coupling than the 57 to 61GHz band. Designing a
chirp to utilize the 61 to 64GHz portion of the frequency band can help lower
the noise figure. Local regulations and other considerations can drive frequency
choice of the end application, but the previous graphs can be used for expected
noise figure in different frequency bands.
- For applications which do not
need all 6 virtual channels (TX and RX combinations), using TX2 can help reduce
noise figure. The coupling is lowest for TX2 in the 59 to 64GHz band. For
single TX applications need, use TX2 over TX1 to get best performance and
maximum range.
- For two TX applications, use TDM MIMO mode instead of BPM MIMO mode.