Figure 4-1 and
Figure 4-2 give the maximum allowed RX gain setting and minimum TX back off restrictions based
on chirp slope (X-axis) and HPF setting (different colors). These are recommendations
which minimize the effects of increased receiver noise figure and risk of receiver ADC
saturation.
TX backoff restriction can be
relaxed as shown in Figure 4-3 for the following cases:
- Chirps contained within 61 to
64GHz for two TX applications
- Chirps contained within 59 to
64GHz for single TX applications (using TX2)
Using the previously-shown
constraints makes sure that the best possible SNR is achieved and also the receiver ADC
is not saturated.