SWRU271I October 2010 – January 2020 CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640R2F
Consider the value of the simpleGATTProfile SIMPLEPROFILE_CHAR1.
The type is set to the custom-defined simpleProfileChar1 UUID (0xFFF1).
Because the properties of this characteristic value are readable and writeable, set the GATT permissions to readable and writable.
NOTE
If the GATT permissions are not set to readable and writable, errors occur.
The pValue is a pointer to the location of the actual value. This value is statically defined in the profile as follows: