SWRU271I October 2010 – January 2020 CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640R2F
You must decide which role and purpose the custom application should have. If the application is related to a specific service or profile, start with one of those. An example application includes the heart rate sensor project. TI recommends starting with one of the following SimpleBLE sample projects:
When deciding the role and purpose of the application, choose from the appropriate libraries in Section 5.8.