SWRU271I October 2010 – January 2020 CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640R2F
The effective connection interval is equal to the amount of time between two connection events, assuming the slave skips the maximum number of possible events if slave latency is allowed. The effective connection interval is equal to the actual connection interval if slave latency is set to zero.
Calculate this interval using the following formula:
Effective Connection Interval = (Connection Interval) × (1 + [Slave Latency])
Where:
When no data is sent from the slave to the master, the slave will transmit during a connection event once every 500 ms.