SWRU271I October 2010 – January 2020 CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640R2F
connHandle: connection to use
pInd: pointer to indication to be sent
authenticated: whether an authenticated link is required
taskId: task to be notified of acknowledgment
If the return status is SUCCESS, the calling application task will receive a GATT_MSG_EVENT message with type ATT_HANDLE_VALUE_CFM upon an acknowledgment. It is only at this point that this subprocedure is considered complete.
connHandle: connection to use
pNoti: pointer to notification to be sent
authenticated: whether an authenticated link is required
If the return status is SUCCESS, the notification has been successfully queued for transmission.