SWRU332C November 2012 – October 2016 CC2540 , CC2541-Q1
The project and source code files for the preprogrammed application (as well as many others) are included with the Bluetooth low energy (BLE) stack from Texas Instruments, which can be downloaded at www.ti.com/ble-stack.
The project implementing this demo is called Keyfobdemo (CC2541DK-mini Keyfob Slave configuration). The project can be modified as desired, and should provide a good framework for developing custom BLE applications.
More details on these projects can be found within the BLE Software Developer’s Guide (SWRU271), which is also included with the stack installer. For troubleshooting, refer to the CC2540/41 Mini Development Kit User Guide (SWRU270).